Dear vkojin,
I apologise - I somehow missed you query when originally posted.
I'm unsure what is happening here. Could you please do the following to help track the fault:
Replace the DLLs with the debug DLLs supplied in the original Zip files.
Try the debugger as before.
The debug DLLs will create a log file in C:\usbdm_dll.log. Please post this log file.
What speed is the MC9S08GT60CFBE operating at?
bye
PS. The MC74HC125N is an unsuitable device since it does not allow operation between systems operating at different voltages. A 74LV125A would be better.
Dear pgo,
here, in Bulgaria, is very difficult to buy jb16 micros, and i already buy jb08.
and, in my case, i need to programm hcs 08 based modules (zigbee modules by Panasonic) and i'm not sure that TBDML work for me.
This project is very urgent for me, where i can find sollution for me?
I assume you mean "... not using the FET..."
"If you are not using the 5V supply you need an external diode instead."
"The BSS188 has a Vgs(th) of ~1V (1.4max) so would be better for low target Vdd."Since I can't get the BSS138, I assume the IRLML2502 is the best replacement: Vgs(th) of 0.6 to 1.2V. A bit overkill.
"The MAX9119 would be suitable I believe but it comes in a very small package?"Indeed, it is a SC70-5, which is just over half the size of SOT23-5.
"This bead isn't really important and could be omitted if not concerned about interference (put a pad in and use a 0-ohm resistor initially)."I'm using a 2-pin jumper footprint at the moment. The jumper would be removed to bypass USB power. I could easily put a low value wired inductor in the spot if circumstances require such.
Dear Pgo,
Thanks for new software, but I still have this same problem. I modified USBDM_JB16.h file for my hardware, compile it, and upload to JB16. I trying it on my MC9S12NE64 using your Test_USBDM.exe and this is result of usage:
settarget 0
Executing:settarget 0
:setTarget 0
speed 25
Executing:speed 25
Setting speed failed
Speed = 25.00 MHz (614 ticks, sync=10.2 us)
connect
Executing:connect
:connect - Failed
Status = Wait, Not Connected, Reset
Speed = 15360.00 MHz (1 ticks, sync=0.0 us)
I can't change speed for hcs12 nad hcs08.
My hardware is identical like presented in this file: TBDML_JB16_SOIC28(Minimal).pdf
I try to compile your software in TBDML mode, but result is the same.
I see something interesting until programming JB16, when I use this: Re-programming_BlockErase.imp and select another software version it not change, but when I use: Initial_Programming_MassErase.imp software in jb16 was changed correctly.
I attache my USBDM_JB16.h file, if you cane pelase check it that is correct for my hardware.
Best Regards,
Maciej Bojczuk
Dear Pgo,
Please tell that is possible to run your USBDM on this hardware:
http://www.freescale.com/files/community_files/OSBDM08/USBDM_JB16_SOIC_JB16JDWE.pdf
(JB16 SOIC20 + 74HCT125)
And my second question is connected with target, USBDM support MC9S08JM60 device?
Best Regards,
Maciej Bojczuk
http://forums.freescale.com/attachments/freescale/TBDML/305/2/USBDM_JB16_SOIC_JB16JDWE.pdf" target="...
Message Edited by pgo on 2008-10-14 03:21 AM
Message Edited by pgo on 2008-10-14 03:23 AM
Message Edited by pgo on 2008-10-28 02:00 AM
Message Edited by pgo on 2008-10-28 02:00 AM
Message Edited by pgo on 2009-02-05 03:18 PM
Dear chiusir,
I'm having trouble understanding what you mean!
Could you try the following (and report results)?
Completely erase the JB16 (using MON08 if necessary).
Confirm ICP operation using the Freescale ICP software. This will confirm the basic USB interface.
Use the ICP software to download the appropriate USBDM image to the JM16.
Reconnect and describe the results!
It is necessary to have the Special Edition: CodeWarrior for Microcontrollers installed for the correct driver to be available. (Not the Special Edition: CodeWarrior for HCS12(X) Microcontrollers version though it will then work with this as well provided the above version is installed as well).
bye
Message Edited by pgo on 2008-12-24 12:31 AM
Message Edited by pgo on 2008-12-24 12:31 AM