Message Edited by lemonmeng on 04-05-200602:22 AM
Hello
The attached Special Edition license file activates the flash programmer. This license file posted on the WEB this week. The flash programmer will be part of the Special Edition V5.1 license file when it is released.
For your information, we will also release a service pack later in the year which will add the Open Source BDM to the connections list. Project has not be scheduled yet, so I cannot give you a date for that.
I Hope this helps.
CrasyCat
When I first started using Codewarrior + Hiwave for HCS12 I had one of the original Motorola Serial BDM interfaces. I had to get them to do a special license so I could use this with over 1k of code. The compiler at that time was limited to 12k for the Free version which worked fine up to the 12k limit. I ran into the same issue when using the Motorola BDM and P&E worked fine.
So I guess what I am saying is that a License change fixed my problem similar to this at the time.
Hi Lemonmeng,
I have noticed this problem as well.
I have exactly the same setup as you.
If you use P&E USB ML 12 to download it uses P&E software and there is no limitation.
But when using the OSBDM it seems to use Hiwave software to download/flash.
If you look in the "about" when in the true time simulator you can see some license info that seems to allude to this limitation.
Hopefully someone "in the know" can help us out here.
I have avoided this issue (by using a small test file) for the time being as I am just trying to qualify a design for a smallest/simplest easy to construct PCB for this BDM. Hence my questions elsewhere about USBICP as I want to leave off MON08 if possible.
BR Peg