MBDToolbox for S12ZVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDToolbox for S12ZVM

12,906 Views
almin_svraka
Contributor I

Hello,

For some time I have been trying to add MBDToolbox for S12 ZVM to Matlab unsuccessfully.
I was able to add MBDToolbox for S12 ZVC to Matlab; however, I need to have a toolbox for S12ZVM in Simulink.
In addition, there is a setup file for S12ZVC toolbox, and it worked fine, but no setup file for S12ZVM.
The script (m file) that comes with NXP_Support_Package_S12ZVMx_20200907 does nothing.
Basically, it runs and at the end it says that the toolbox was added, but it is not added- No MBDToolbox in Simulink.

I tried with Matlab 2020b and Matlab 2020a and it doesn't work for neither.

Please advise !

Almin

Tags (1)
0 Kudos
Reply
22 Replies

12,640 Views
constantinrazva
NXP Employee
NXP Employee

Hello @almin_svraka ,

Can you try do the following and see if this works on your end?

1) Go to https://www.nxp.com/design/automotive-software-and-tools/nxp-model-based-design-toolbox-mbdt:MBDT link

 

2) Click on Download button (at this step you will be prompted to log into your nxp.com account)

constantinrazva_0-1605023753621.jpeg

 

 

 

3) After you logged in, select the following from the list: Model-Based Design Toolbox for S12ZVMx Automotive Microprocessors Family

constantinrazva_1-1605023753716.jpeg

 

 

4) Click on “I Agree”

 

5) download the MBDToolbox_S12ZVMx_1.4.0_20200909.mltbx file

constantinrazva_2-1605023753791.jpeg

 

6) The file will be automatically saved as .zip – just rename the file to .mltbx [from MBDToolbox_S12ZVMx_1.4.0_20200909.zip to MBDToolbox_S12ZVMx_1.4.0_20200909.mltbx]

 

7) Open MATLAB – run the MBDToolbox_S12ZVMx_1.4.0_20200909.mltbx file

 

After you finish the installation process from MATLAB, you should be able to see the ZVM toolbox installed.

There is a big difference between the older ZVC toolbox and the updated ZVM one when it comes to installation - we switched to this mltbx as it is a Mathworks installation technology and we try to achieve a deeper integration within MATLAB/Simulink.

 

Kind regards,

Razvan.

0 Kudos
Reply

6,131 Views
gary_lu1
Contributor II

Hi,I have the same questions,the MBD toolbox for SZ12ZVMx can not install successfully although I try any ways,My matlab version is R2021a,I want to know if this toolbox support the newer version than R2020a?

12,633 Views
almin_svraka
Contributor I

Hello,

I did it as you said to do it - followed the steps - it doesn't work

Basically, Matlab 2020a says the toolbox is added - when I run command "ver"

MATLAB Version 9.8 (R2020a)
Simulink Version 10.1 (R2020a)
Embedded Coder Version 7.4 (R2020a)
IEC Certification Kit Version 3.15 (R2020a)
MATLAB Coder Version 5.0 (R2020a)
Model-Based Design Toolbox for S12ZVMx Series Version 1.4.0 (R2015a-R2020a)
Simulink Coder Version 9.3 (R2020a)
Stateflow

When I open Simulink browser - nothing is there (empty)

Please advise !

 

 

0 Kudos
Reply

12,604 Views
constantinrazva
NXP Employee
NXP Employee

Hello @almin_svraka ,

If you open the Simulink library browser (see MATLAB command below), you do not see the NXP Model-Based Design Toolbox for S12ZVMx ?

slLibraryBrowser

 

Note that it should be the first one and not alphabetically ordered.

 

Kind regards,

Razvan.

0 Kudos
Reply

12,598 Views
almin_svraka
Contributor I

Hello,

No, I don't see it - it is not there

I have:

  • Simulink
  • Embedded Coder
  • HDL Coder
  • Simulink 3D Animation
  • Simulink Coder
  • Simulink Extras
  • Stateflow

 

Please Advise !

Almin

0 Kudos
Reply

12,578 Views
constantinrazva
NXP Employee
NXP Employee

Hello @almin_svraka ,

Can you let me know if you can see it in the Add-on Manager?

constantinrazva_0-1605181689998.png

 

If that exists, can you run the following command in MATLAB terminal:

mbd_find_s12z_root

If that returns a path, please go to that path and open an example from S12ZVM_Examples folder. 

 

One more thing - after you open slLibraryBrowser, can you refresh it? You can press F5 for that. Maybe that will do the trick.

 

Kind regards,

Razvan.

0 Kudos
Reply

12,572 Views
almin_svraka
Contributor I

Hello,

Yes, I can see it it in Add-On Manager - image attached

Yes, there is a return path after mbd_find_s12z_root is ran and it is:

'C:\Users\almin.svraka\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx'

Yes, I can open an example; however, all S12ZVM blocks are in red (not recognized) - image attached

Refreshing Simulink Library doesn't help - image attached

Restarting Matlab doesn't help !

Restarting Windows doesn't help !

 

Please Advise !

Almin

 

0 Kudos
Reply

12,562 Views
constantinrazva
NXP Employee
NXP Employee

Hello @almin_svraka ,

 

Unfortunately I can only see your first image - I must mention that the blocks are indeed recognized, as if they were not, you would have not been able to see information displayed on NXP blocks. You should try and build any example to make sure it all works out. If you haven't yet setup your license, you can read the documentation and follow the steps from there or from various community posts about it.

 

Regarding the other issue with the library not being visible in the browser, I'm not yet sure why this is happening - I'm trying to reproduce your issue on various setups, but to no avail. I can see it on every setup I've tried so far. Will get back to you on this aspect, but in the meanwhile test out examples and let me know if those build or not.

 

Kind regards,

Razvan.

0 Kudos
Reply

12,556 Views
almin_svraka
Contributor I

Hello,

Would you please show me (take a screenshot and post it here) the MBDToolboox for S12ZVM in your Matlab2020a/Simulink browser ?

 

Best Regards,

Almin

0 Kudos
Reply

12,521 Views
constantinrazva
NXP Employee
NXP Employee

Hello @almin_svraka ,

As you can see in the image below, on whatever setup I ran the installer on, I got it visible in the Simulink library browser.

constantinrazva_0-1605529730283.png

 

Can you show us what errors you are getting when trying to build an example?

 

Kind regards,

Razvan.

 

0 Kudos
Reply

12,509 Views
almin_svraka
Contributor I

Hello,

I tried to run the first example, adc_s12zvm, from the Example directory.

I attached the screenshot from Simulink/Embedded Coder screen.

Best Regards,

Almin

0 Kudos
Reply

12,502 Views
constantinrazva
NXP Employee
NXP Employee

Hello @almin_svraka ,

 

Can you also send us the error you are getting?

 

Kind regards,

Razvan.

0 Kudos
Reply

12,495 Views
almin_svraka
Contributor I

Hello,

I installed then uninstalled then installed (many times) MBDToolboox - just trying to see if something is skipped during the installation.

Anyways, the error message for that particular example this time (just ran a few minutes ago) is attached to this message.

The directory path is: C:\Users\almin.svraka\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\adc

Best Regards,

Almin

0 Kudos
Reply

12,479 Views
almin_svraka
Contributor I

The expanded is attached too.

Almin

 

0 Kudos
Reply

12,473 Views
paulvlase
NXP Employee
NXP Employee

Hi @almin_svraka ,

 

Can you run the following commands:

1. cd(mbd_find_s12z_root())

2. mbd_s12z_path()

3. sl_refresh_customization()

4. build the adc_s12zvm example

 

and post any warning or error you get.

 

0 Kudos
Reply

12,435 Views
almin_svraka
Contributor I

It builds now.

0 Kudos
Reply

12,431 Views
almin_svraka
Contributor I

Hello,

Actually, this is the output:

>> cd(mbd_find_s12z_root())
>> mbd_s12z_path()
Treating 'C:\Users\almin.svraka\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx' as MBD Toolbox installation root.
MBD Toolbox path prepended.
Successful.
>> sl_refresh_customization()
Unrecognized function or variable 'sl_refresh_customization'.

Did you mean:
>> sl_refresh_customizations()

 

Yes, it build with some warnings.

### Created executable: adc_s12zvm.elf Building target all *** Created executable: adc_s12zvm.elf ### Successful completion of build procedure for: adc_s12zvm ### Simulink cache artifacts for 'adc_s12zvm' were created in 'C:\Users\almin.svraka\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\adc_s12zvm.slxc'.

 

0 Kudos
Reply

12,423 Views
paulvlase
NXP Employee
NXP Employee

Yeah, it is sl_refresh_customizations(), with an 's' at the end. But you don't need to run it anymore, now that it works to build the adc_s12zvm model.

 

That message is a confirmation that the elf executable was build successfully.

 

 

12,210 Views
almin_svraka
Contributor I

Yes, the example, adc_12zvm, builds from the Examples directory.

However, that is not the solution to the problem - MBDToolbox for S12ZVM is not visible in Simulink library

Best Regards,

Almin

 

0 Kudos
Reply

12,520 Views
constantinrazva
NXP Employee
NXP Employee

One thing I want to clarify - when I'm talking about license, I am talking about the license for our toolbox - the license that can be accessed from the nxp.com website. This license is different from the MATLAB/Simulink license.

 

Kind regards,

Razvan.

0 Kudos
Reply