How to reset/initialize Ramp/PI-Control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to reset/initialize Ramp/PI-Control

1,469 Views
nofake_drstrang
Contributor III

Hello,

because with "S12ZVM_FOC_Sensorless.slx", everytime when supply power is ON, the motor spins with request speed. There is no Stop-mode.

So I want to build the Stop-mode. But how can I reset/initialize the PI-control/ramp internal states ?

pastedImage_1.png

Thanks in advance!

4 Replies

1,380 Views
nofake_drstrang
Contributor III

Hi,

I change the mask to:

pastedImage_1.png

Maybe you have another better/correct way to share.

Many thanks!

0 Kudos
Reply

1,380 Views
constantinrazva
NXP Employee
NXP Employee

Hello nofake.drstrange ,

We will have an update for the ZVM toolbox on September 7th (just around the corner) - and we'll be updating the AMMCLib blocks with the new version; there you'll have an easy way to reset it.

Kind regards,

Razvan.

1,360 Views
nofake_drstrang
Contributor III

Hi, 

do you know when the new tool box released?

 

Thanks in advance!

0 Kudos
Reply

1,380 Views
mariuslucianand
NXP Employee
NXP Employee

paulvlase‌, can you comment on this?

Regards,

Marius

0 Kudos
Reply