NXP FTF 2016 - トレーニングプレゼンテーション

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP FTF 2016 - Training Presentations

ディスカッション

ソート順:
Today’s designers are facing ever increasing challenges to protect their intellectual property and products from counterfeiting or unauthorized access. To help customers better understand the solutions offered by NXP, Future’s System Design Center has designed a Secure Access Demo board to showcase the capabilities of the LPC43S57, a microcontroller with integrated security, and the A700X, a tamper resistant secure MCU solution. This class will present an overview of the architecture of a secured system and provide an introduction to the secured elements from NXP. Watch Video Presentation
記事全体を表示
Embedded Planet designed the new NXP LS1043 Gateway. Come learn the details of the hardware and software designed for this next generation residential Gateway.
記事全体を表示
This session will provide a detailed introduction to NXP's HomeKit Software Development Kit (SDK) architecture, APIs and code adaptors. Through hands-on examples, you will learn accessory profile configurations, how to integrate with accessory application software, and how to build and debug a demo accessory (Restricted to verified MFi licensees only).
記事全体を表示
In designing cooking appliances, there is ample consideration given to power required from a home's wired electrical system as well as the performance needed to maintain safety and operating temperatures. NXP's solid state RF cooking team has partnered with Wayv Technology to develop a portable food heating appliance using solid state RF energy. This session will cover the key challenges and approaches to delivering energy to heat food in a portable, on-the-go appliance. Watch Video Presentation
記事全体を表示
There are many variables to consider when implementing and integrating solid state RF power into a cooking appliance. Cavity size and shape, RF feed type, power, thermals, and configuration all factor into design consideration. This session will cover key consideration and methods of simulating to achieve better system design. Watch Video Presentation
記事全体を表示
NXP introducing the most comprehensive smart home/IoT Evaluation kit enabling multiple technologies as wireless connectivity, security & NFC commissioning with audio features. NXP's complete value proposition combines to give best user experience, performance and accuracy to develop best home/building automation solutions.
記事全体を表示
Hands-on training for ZigBee-3.0 with NXP lowest power Wireless MCU, using evaluation kit. Quickest and fastest way to develop a smart home product using ZigBee-3.0 such as sensors, monitoring device panels, router devices and Gateway solutions.
記事全体を表示
Lecture on NFC commissioning and various use-cases NFC enables in Smart Home/IoT to save cost and enable convenience. NFC gives best of user experience for installing devices in Smart Home & Buildings and in-addition also useful for Diagnostic, de-commissioning, OTA upgrade and various other useful features.
記事全体を表示
This hands-on workshop provides a detailed architecture description of Thread technology and wireless mesh networking. The main Thread concepts will be reviewed and analyzed thoroughly. The attendee will have a deep understanding of the main concepts and how these are mapped to the NXP software API. The session will close with hands-on training to enable the attendee to understand software usage and configuration, low-power features and security concepts.
記事全体を表示
The Kinetis KE1x family is the next generation MCU solution in the Kinetis E series. Designed with more memory, enhanced features and new IPs, this family extends the NXP 5 V portfolio to cover higher performance applications and use cases. Together with the Kinetis KE0x family for entry level MCUs, the Kinetis E family becomes an ideal solution for markets needing 5 V, robustness, and more flash size, providing platform solutions for low-end to high-end applications. Join this session to learn how the strong EMC performance across the Kinetis E family makes it suitable for main control and HMI (touch) in home appliances, industrial, and other applications needed in harsh electrical noise environments. Watch Video Presentation
記事全体を表示
Companies and consumers alike are excited about the opportunities offered by the IoT and the Smart Home. Concerns on user-friendliness and security are however holding potential customers back: how can I install it? , what if my neighbor hacks into my network? NFC technology addresses these cost, ease of use and security concerns by offering short distance out-of-band pairing capabilities that reduce the complex commissioning system to a simple 'tap'. And with NXP's connected NFC tag technology, IoT nodes of all sizes do not even need to be powered. Watch Video Presentation
記事全体を表示
Experience the power of market leading real time operating system, FreeRTOS and Kinetis MCUs. Learn with experts about the FreeRTOS and how to enable FreeRTOS on Kinetis MCU's: Creating a Kinetis SDK project with FreeRTOS and Kinetis Design Studio, configure it for best code size and performance, debug it with Kernel Awareness in Eclipse and how to get detailed application and systems performance data using FreeRTOS+Trace performance analysis tools.
記事全体を表示
Many customers struggle getting their first GUI design running, and often this results in schedule and budget problems. This class covers the issues and SOLUTIONS required to get a Graphical User interface up and running. We provide solutions to standard embedded communication requirements like Ethernet, USB, Wi-Fi, and Serial. We present a Case Study of a new product using a touch screen GUI, LEDs and audio to communicate the fluid level and temperature of a beverage container back to the user. We cover the pros and cons of developing your own software or of using proven off-the-shelf solutions based on standard building blocks. We also address the buy vs. make hardware decision and look at time to market and risk factors. The class ends with a demonstration of the solution implemented with an off-the-shelf NXP LPC microcontroller based hardware module and simple custom expansion board.
記事全体を表示
This presentation will demonstrate the capabilities of the new i.MX 7 System-on-Chip, a hybrid solution containing a Cortex-A7 processor and a Cortex-M4 processor. Particular attention will be given to the hardware modules and software counterparts allowing both cores to communicate with each other. This hybrid architecture will be highlighted through various potential use cases/product scenarios and a Qt powered application running on top of Linux along with FreeRTOS will be showcased, focusing on asymmetric processing.
記事全体を表示
To use the processor in an integrated design is one way. To use an embedded module is another way and will speed up the design, reduce the design risk and lower the design cost. What support will be offered by the different module suppliers? What limitations and restrictions are there, if you use an embedded module? A market overview and guideline to select your embedded module supplier.
記事全体を表示
IoT applications often share some basic requirements; the applications themselves need to be small, fast and low-energy, while the time to market should be as short as possible. To help you meet these demands, a wide range of possibilities and techniques for performing smart debugging of code is actually already at your fingertips. At this session you will learn how to use debug features like various types of complex breakpoints, macros, stack checking, event logging, live data, profiling and runtime code analysis in a smart way for comprehensive debugging of your code.
記事全体を表示
Near Field Communications (NFC) is appearing on many new smartphones, and offers secure money transactions (Apple Pay and Google Wallet) and convenient access to public transport or even your hotel room. NXP's NFC receiver is a key component that enables mobile NFC hardware. Today we'll talk about how to get more from your NFC experience by boosting the Smartphone battery voltage, or reducing the NFC antenna size - for more stylish slim phones - while not upsetting other circuits in the phone with unwanted RF noise.
記事全体を表示
The new USB TYPE-C and PD specification has brought the new possibilities on power implementation through USB port, that will give the end customer a very different experience. At the same time, the new specification has raised the requirements on the power components with higher voltage and higher current. Also the ability to swap current source and change output voltage makes the power structure design even more complex. In order to distribute power in a reliable way on TYPE-C port, NXP has developed a set of Power switches for it. Watch Video Presentation
記事全体を表示
This session introduces designers to authentication of USB devices, including use cases such as high power charger authentication over USB PD, and the solutions to threats posed by "Bad USB". Approaches covered will include pros and cons of vendor-specific authentication as well as compliance with emerging standards. Specific implementation examples will be discussed using NXP authentication products within the USB Type-C ecosystem. Watch Video Presentation
記事全体を表示
Industry 4.0, also known as Industrial IoT, is based on cyber physical systems. It will connect objects together inside and outside the factory. This session will discuss the newest technology solutions to access up to the far end remote node via wired or wireless connection. We will go into more detail on IO-Link, a point to point communication, replacing traditional sensor to PLC cabling. IO-Link enables smart access to a sensor or an actuator with data collection and maintenance capabilities. We will also look at disruptive long range wireless communication based on Sigfox technology to connect isolated sensors requiring a long battery life. Watch Video Presentation
記事全体を表示