NXP FTF 2016 - トレーニングプレゼンテーション

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP FTF 2016 - Training Presentations

ディスカッション

ソート順:
Automotive applications based on modern processor technology require more complex hardware design than traditional microcontroller solutions: volatile and non-volatile memories are provided external to the device and multiple power supplies are required. This session provides a guide to developing a hardware platform using the S32V234 processor as an example. Topics covered include: power supply design considerations, memory layout and technology, camera and display connectivity, fast interface technology and serial bus physical interfaces. Watch Video Presentation
記事全体を表示
Though cryptographic algorithms like AES are crypto-analytically secure, real implementations must at least be tested against logical attacks such as API misuse. Smart cards and similar devices also face fault and side channel attacks. Such attacks exploit physical effects to manipulate the device or learn about secret information. As these attacks are very critical, customers in the smart card industry ask for third party evaluation (e.g. Common Criteria or EMVCo) to confirm high assurance levels. If passed, a certificate is issued by a trusted party. With the rise of the IoT, physical attacks and respective third-party witnessing of resistance might soon be relevant there as well. Watch Video Presentation
記事全体を表示
Advancing technology has brought down the cost of 24 GHz radar system significantly bringing a whole range of new applications into reach. Historically radar was a pure military and industrial application due to high application costs. With the latest generation of NXP BiCMOS technology this has changed. A 24 GHz radar frontend can now be fully integrated into a single IC bringing the costs and power dissipation down to consumer levels. This opens up a whole range of applications which were previously not possible. This lecture will show the possibilities of radar in different applications such as presence detection and consumer drone collision avoidance. A live demonstration based on first test chips in combination with ARM processors will be given.
記事全体を表示
This presentation will present a simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC.
記事全体を表示
Exploration of the use cases and applications that are ideal for the DPAA2, including vCPE, UTM, the intelligent edge, Top-of-Rack switching and storage.
記事全体を表示
This will be a hands-on session covering the Kinetis Software Development Kit (SDK) and Kinetis Expert using the Kinetis Design Studio Integrated Development Environment (IDE).  
記事全体を表示
Charging smartphones without the need to plug in a charging wire increases convenience and enables on-the-move charging in public spaces. First generation wireless chargers consist of over 100 components and are too expensive for mass market adoption. The NXQ1TXH5 is a one-chip Qi low power wireless charging transmitter integrating all the digital, analog and power functions for a Qi wireless charger. The high integration enables a very low component count and an easy to design wireless charger. This also reduces the cost of a wireless charger by as much as a factor 3. The NXQ1TXH5 is a real digital plug & play platform without the need for external analog design effort. A 2-layer PCB with signal & power routing at the top layer and a full copper bottom layer for thermal performance is all you need. Connect power supply and decoupling at the input and an LC circuit at the output to transmit the power to the receiver, and your wireless charger is ready to go! Watch Video Presentation
記事全体を表示
Get a deep dive into the brand new Vulkan API from Khronos. Learn how the programming paradigms have changed from OpenGL ES, how to use Vulkan API and its enormous performance advantages, and how to unlock the full potential of i.MX 8 series GPUs. Watch Video Presentation
記事全体を表示
Wayland and Weston are gaining popularity as Window Manager and Compositor on Linux, and they are part of our reference board support package (BSP). This lesson dives deep into the setup of Wayland/Weston on custom BSPs, enabling xWayland, and successful configuration of advanced multi-display and multi-input setups on i.MX applications processors.
記事全体を表示
In this session, Linear Technology will provide detailed design guidelines for robust and scalable power solutions for the latest QorIQ processors. Using proven NXP reference design examples for the T1023, LS1043, LS1046 and LS1088 this session will explore the key considerations of each design and show you how to leverage and scale the reference designs for your applications.
記事全体を表示
As connected edge devices gain momentum with consumers, the security approaches and assumptions of the past will fail and create new threats and vulnerabilities to consumer safety and privacy. Additionally, the cost for security in mobile phones, tablets, and PCs will present a challenge for applications such as occupant sensors and heart rate monitoring patches. Lastly, the teams of security experts in connected industries do not yet exist at suppliers who are connecting products to the network. Join this session to learn how industries are providing cost effective, highly secure, certified hardware that can hasten the learning cycle for emerging edge node applications, bring solutions for security, drive down costs, and limit the supplier specific required expertise.
記事全体を表示
This beginning hands-on session will walk you through the steps to configure the device and boot U-Boot. Learn how to configure the device reset control word (RCW), flash the device, and debug U-Boot. This session will use the CodeWarrior Development Studio for ARM®v8 ISA to boot the QorIQ LS1021A Reference Design Board (RDB).
記事全体を表示
With the trend of frequent and remote software updates on the vehicle, the need of managing this properly at the microcontroller is critical. This session will present the challenges on microcontroller reprogramming and how our S32K144 microcontroller properly addresses it safe and efficiently.
記事全体を表示
The CodeWarrior Development Suite for the QorIQ LS series includes a variety of tools targeted at analyzing the operation and performance of a multicore Linux system. Tools utilitize hardware trace and system logs to monitor operation and performance. CodeWarrior Development Suite includes tools for performance analysis with the Hierarchical Profiler, Flat Profiler and CodeCoverage; path analysis with Timeline and CallTree; real-time monitoring with DebugPrint and TraceCommander in addition to interval profiling.
記事全体を表示
The I2C bus has expanded from its humble beginnings in 1980s home electronics to both small and large scale systems in the modern world. Applications range from Smartphones to Server farms, and while they're true to the original simple signaling protocol other I2C bus components are needed to expand, adapt or buffer those signals. We take an in depth technical look at the simple Bus Buffer. Often needed, and seldom understood. Watch Video Presentation
記事全体を表示
Designer have a simple way to achieve functional safety standards with NXP's functional safety microcontroller portfolio. During this session we will cover how functional safety applies to both the automotive and industrial markets and the support NXP offers in each step. Watch Video Presentation
記事全体を表示
From solving a simple problem - How did a 1980s TV 'talk' to your new Video Cassette Recorder (VCR)? - The Inter-Integrated Bus has solved many of today's low speed communication problems. Known affectionately as the I2C (pronounced eye-squared-see) bus, just two wires can connect a variety of electronic components that help us enjoy many products from Smartphones to Cloud Server farms. In industry the I2C bus is a simple and reliable link for sensors, indicators, human interface, and behind-the-scenes equipment set up and control. We talk about how it works, and what it can do for your next electronics project. Watch Video Presentation
記事全体を表示
This is an overview of the next generation S32K microcontrollers family and the system solution benefits using the latest MCU features. Watch Video Presentation
記事全体を表示
Deep dive into the vision processing architecture of the i.MX 8 family. Learn how to access the advanced processing features, the vision SDK, and the vision-based applications enabled by the i.MX 8 processor. This class provides an introduction to understanding the unique way in which machine vision is handled by i.MX 8. It forms a basic introduction class that is a precursor to the more advanced "Call Your Shot!" pool table demo class. Watch Video Presentation
記事全体を表示
The standard CAN protocol has been extended into CAN Flexible Data (FD) to provide higher bandwidth while keeping the physical characteristics that have made it the most popular automotive in-vehicle communications protocol . This presentation will provide an overview of the changes to the standard as well as address the challenges faced while rolling out and implementing the technology. Watch Video Presentation
記事全体を表示