NXP’s 1500 W MRF1K50 RF Power Transistor Benchmark

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP’s 1500 W MRF1K50 RF Power Transistor Benchmark

NXP’s 1500 W MRF1K50 RF Power Transistor Benchmark

Demo

NXP has released the 1500 W MRF1K50H and MRF1K50N. The industry’s highest power transistors for ISM, FM broadcast and sub-GHz aerospace applications. These are pin-compatible so can be situated on the same PCB as existing solutions on the market

Demo / product features

MRF1K50H 1.5 kW LDMOS Transistor

  • 1–500 MHz, 1500 W CW
  • 74% efficiency
  • 23.5 dB gain
  • Extremely rugged  (65:1 VSWR)

MRF1K50N 1.5 kW LDMOS Transistor

  • 1–500 MHz, 1500 W CW
  • 73% efficiency
  • 23 dB gain
  • 30% lower thermal resistance compared to ceramic package
  • Extremely rugged  (> 65:1 VSWR)

NXP Recommends

pastedImage_0.png

Labels (1)
Tags (2)
No ratings
Version history
Last update:
‎05-24-2016 02:16 PM
Updated by:
NXP Employee