unusable keys in ntag 424 dna

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unusable keys in ntag 424 dna

612件の閲覧回数
zahra2023
Contributor III

Hi,

I am developing an app for R/W on Ntag424 DNA and I don’t use any hardware (as NFC Reader) so I myself config the NFC and run commands . The problem is that I am facing issues with the keys becoming unusable after a while of working on tags and returning null. According to section 7.4, Failed Authentications Counter, in the AN12196 PDF, it would be possible that the problem is :

"TotFailCtr (2 bytes)
– Increases by 1 on each unsuccessful authentication
– Decreases by value defined with TotFailCtrDecr
when TotFailCtrLimit is reached, related key cannot be used for Authentication anymore"

BR.

 
タグ(2)
3 返答(返信)

544件の閲覧回数
KellyLi
NXP TechSupport
NXP TechSupport

Hello @zahra2023 

For your issue, below is the part of the log for your reference, which could be helpful to you.

KellyLi_0-1697793723647.png

BR

kelly

0 件の賞賛
返信

534件の閲覧回数
zahra2023
Contributor III

Thanks for your reply @KellyLi , but I want to know the reason of my problem (why the keys become unusable after a while). Now I can run authentication and other commands except the one I posted here: https://community.nxp.com/t5/NFC/SetConfiguration-Command-return-error/td-p/1743977

I would really appreciate if you could help me.

BR.

0 件の賞賛
返信

484件の閲覧回数
KellyLi
NXP TechSupport
NXP TechSupport

Hello @zahra2023 

Since you are not designing based on one hardware, where are your keys stored? In general, the key used for authentication is stored at the end of the card reader。 So is this what's causing your KEY to be unstable?

BR

kelly

0 件の賞賛
返信