unusable keys in ntag 424 dna

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unusable keys in ntag 424 dna

1,094 Views
zahra2023
Contributor III

Hi,

I am developing an app for R/W on Ntag424 DNA and I don’t use any hardware (as NFC Reader) so I myself config the NFC and run commands . The problem is that I am facing issues with the keys becoming unusable after a while of working on tags and returning null. According to section 7.4, Failed Authentications Counter, in the AN12196 PDF, it would be possible that the problem is :

"TotFailCtr (2 bytes)
– Increases by 1 on each unsuccessful authentication
– Decreases by value defined with TotFailCtrDecr
when TotFailCtrLimit is reached, related key cannot be used for Authentication anymore"

BR.

 
Tags (2)
3 Replies

1,026 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @zahra2023 

For your issue, below is the part of the log for your reference, which could be helpful to you.

KellyLi_0-1697793723647.png

BR

kelly

0 Kudos
Reply

1,016 Views
zahra2023
Contributor III

Thanks for your reply @KaiLi , but I want to know the reason of my problem (why the keys become unusable after a while). Now I can run authentication and other commands except the one I posted here: https://community.nxp.com/t5/NFC/SetConfiguration-Command-return-error/td-p/1743977

I would really appreciate if you could help me.

BR.

0 Kudos
Reply

966 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @zahra2023 

Since you are not designing based on one hardware, where are your keys stored? In general, the key used for authentication is stored at the end of the card reader。 So is this what's causing your KEY to be unstable?

BR

kelly

0 Kudos
Reply