I modify the " Using-NFC-Reader-Library-with-LPC55S69 " from CLR663 to PN5180.
I setting the config. but still show the error message " Error - (0x 101) has occurred in NFCLIB "
or How to transplant the NFC reader library 5.22 to LPC55S69?
Hello,
Sorry for the late response, could you please confirm that you disconnected/short-cut the connections from the LPC that is on board ? Also, could you please confirm that the device does not starts with a 1 in the DWL pin ?
Regards ,
Estephania
Hello,
Could you please help me with a picture of the board connections? Just to confirm, the only change you made was the usage of the library or did you only change the HAL in the library ?
Regards,
Estephania
I using the LPC55S69 EVK and PNEV5180B demo board.
SPI
CS -- port1, pin1
SCK -- port1, pin2
MISO -- port1, pin3
MOSI -- port0, pin26
Busy ---- port1, pin4
IRQ ------ port1, pin23
DWL ----- port1, pin24
BUSY----- port1, pin25
I changed the usage of the library.
follow the " NFCReaderLibrary_IMXRT1050_CLEV6630B_Porting Guide.pdf " step.