Using External Circuits with the PN5180 or PN5190

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using External Circuits with the PN5180 or PN5190

522 次查看
akihiro-sugiura
Contributor I

CLRC 663 allows you to:
It outputs a modulated signal from SIGOUT and sends it to the card using a proprietary analog transmission circuit.
The card's response is binarized using a proprietary analog receiving circuit, and this binarized signal is input to SIGIN to demodulate the card's response.

If I do the same thing with PN 5190, what is the pin number that corresponds to SIGOUT or SIGIN?

0 项奖励
回复
0 回复数