Using External Circuits with the PN5180 or PN5190

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using External Circuits with the PN5180 or PN5190

463 Views
akihiro-sugiura
Contributor I

CLRC 663 allows you to:
It outputs a modulated signal from SIGOUT and sends it to the card using a proprietary analog transmission circuit.
The card's response is binarized using a proprietary analog receiving circuit, and this binarized signal is input to SIGIN to demodulate the card's response.

If I do the same thing with PN 5190, what is the pin number that corresponds to SIGOUT or SIGIN?

0 Kudos
Reply
0 Replies