Use the package NxpNfcRdLib in PN7462AU-FW_v05.02.01_Full to join the PN7462AU_ex_phExRf project can not find the following function:
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_FieldOff (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_FieldOn (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_FieldReset (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_GetExtFieldStatus (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_LPCD (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_LoadProtocol_Initiator (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_RegCallBack (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_SetConfig (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_Exchg (referred from phexrf_15693.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_SetExchgFdt (referred from phexrf_15693.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_LoadProtocol_Target (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_MFC_Disable (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_ExchgISO14443A_ACFrame (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_ExchgISO14443A_ShortFrame (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_ExchgISO14443A_StandardFrame (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_ExchgMFC_Auth (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_Receive (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_Transmit (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_AutoColl (referred from phexrf_cm.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_DeInit (referred from phflashboot.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_Init (referred from phflashboot.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_SetIdleState (referred from phhalpmu.o).
Hi Xia Shuang,
I can compile this project well, see below:
I guess maybe you didn't import some projects into the same workspace.
Please check the following and compare with your workspace.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Shuang,
I am sorry, but so far just lib version is available.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------