Transmission of an int with NDEF (NHS3152)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transmission of an int with NDEF (NHS3152)

1,396 Views
achraf_kabbabi
Contributor II

Hi everybody,

I am using a NHS3152 and I want to readout the analog values of an external resistor connected between the pins ANA0_0 and VSS (in "real-time", let's say 100Hz) and transmit it through a NDEF message.

I am trying first to test the NFC transmission before implementing the readout of the sensor.

I'm sending a simple integer for testing : int adcInput=123456789;

Here is my code in LPCXpresso :

#include "board.h"
#include "ndeft2t/ndeft2t.h" // For NFC communication : NDEF messages
#include <stdio.h>
#include <string.h>
#include <stdlib.h>


int main(void)
{
Board_Init();

// 1. ADC Single-shot

// int adcInput;
// Chip_ADCDAC_Init(NSS_ADCDAC0);
// Chip_IOCON_SetPinConfig(NSS_IOCON, IOCON_ANA0_0, IOCON_FUNC_1);
// Chip_ADCDAC_SetMuxADC(NSS_ADCDAC0, ADCDAC_IO_ANA0_0);
// Chip_ADCDAC_SetInputRangeADC(NSS_ADCDAC0, ADCDAC_INPUTRANGE_WIDE);
// Chip_ADCDAC_SetModeADC(NSS_ADCDAC0, ADCDAC_SINGLE_SHOT);

// // Readout ADC
// Chip_ADCDAC_StartADC(NSS_ADCDAC0);
// while (!(Chip_ADCDAC_ReadStatus(NSS_ADCDAC0) & ADCDAC_STATUS_ADC_DONE)) {
// ; /* Wait until measurement completes. For single-shot mode only! */
// }
// adcInput = Chip_ADCDAC_GetValueADC(NSS_ADCDAC0);

int adcInput=123456789;

// 2. Conversion int to hexadecimal string
char str_adcInput[16];
itoa(adcInput, str_adcInput, 10);

// 3. Sending the NDEF message to the common memory
uint8_t instanceBuffer[NDEFT2T_INSTANCE_SIZE] __attribute__((aligned (4)));
uint8_t messageBuffer[NFC_SHARED_MEM_BYTE_SIZE ] __attribute__((aligned (4)));
NDEFT2T_CREATE_RECORD_INFO_T createRecordInfo;
uint8_t locale[] = "en";
uint8_t payloadText[16];
strcpy((char *)payloadText,(const char *)str_adcInput);
/* Ensure initialization of the NFC HW block is done first. This needs to be done only once.
* Any previously written NDEF message will be lost as the NFC shared memory will be re-initialized.
*/
Chip_NFC_Init(NSS_NFC);
NDEFT2T_Init(); /* Required once, not for every message creation or parsing. */
NDEFT2T_CreateMessage((void*)instanceBuffer, messageBuffer, NFC_SHARED_MEM_BYTE_SIZE, true);
createRecordInfo.shortRecord = 1; /* Enable Short record */
createRecordInfo.pString = locale;
if (NDEFT2T_CreateTextRecord((void*)instanceBuffer, &createRecordInfo)) {
/* The payload length to pass excludes the NUL terminator. */
if (NDEFT2T_WriteRecordPayload((void*)instanceBuffer, payloadText, sizeof(payloadText) - 1)) {
NDEFT2T_CommitRecord((void*)instanceBuffer);
}
}
NDEFT2T_CommitMessage((void*)instanceBuffer);

return 0;
}

I get the following readout on MATLAB using an Adafruit PN532 (programmed with an arduino using the script ntag2xx_read):

Hello!

Found chip PN532
Firmware ver. 1.6
Waiting for an ISO14443A Card ...
Found an ISO14443A card
UID Length: 7 bytes
UID Value: 0x04 0x23 0xC0 0x00 0x62 0x0B 0x04

Seems to be an NTAG2xx tag (7 byte UID)
PAGE 00: 04 23 C0 6F .#⸮o
PAGE 01: 00 62 0B 04 .b..
PAGE 02: 6D 48 07 00 mH..
PAGE 03: E1 11 42 00 ⸮.B.
PAGE 04: 01 03 E8 0E ..⸮.
PAGE 05: 46 FD 01 00 F⸮..
PAGE 06: 03 16 D1 01 ..⸮.
PAGE 07: 12 54 02 65 .T.e
PAGE 08: 6E 31 32 33 n123
PAGE 09: 34 35 36 37 4567
PAGE 10: 38 39 00 34 89.4
PAGE 11: A9 D7 EB 98 ⸮⸮⸮
PAGE 12: FE 54 07 7D ⸮T.}
PAGE 13: 44 ED 2D F4 D⸮-⸮
PAGE 14: 17 CC 1C 05 .⸮..
PAGE 15: 9A BE E1 43 ⸮⸮⸮C
PAGE 16: 69 FF DB 73 i⸮⸮s
PAGE 17: 4D FD F5 7C M⸮⸮|
PAGE 18: 75 3F 9B 53 u?⸮S
PAGE 19: 96 95 5A 4A ⸮⸮ZJ
PAGE 20: 81 7F 0F 6E ⸮.n
PAGE 21: 8E 9B BE 42 ⸮⸮⸮B
PAGE 22: 6C FE ED F0 l⸮⸮⸮
PAGE 23: C5 B0 02 2B Ű.+
PAGE 24: E7 A7 6D D0 ⸮m⸮
PAGE 25: 6B CC 82 97 k̂⸮
PAGE 26: 16 AF 48 11 .⸮H.
PAGE 27: 57 EA 0C 6F W⸮.o
PAGE 28: E9 32 20 DF ⸮2 ⸮
PAGE 29: E3 79 8C E5 ⸮y⸮⸮
PAGE 30: 53 12 DE EA S.⸮⸮
PAGE 31: B7 BB C6 50 ⸮⸮⸮P
PAGE 32: E7 BC A2 B1 缢⸮
PAGE 33: B2 B6 22 B5 ⸮⸮"⸮
PAGE 34: 78 3E A4 76 x>⸮v
PAGE 35: 3F 58 C8 0B ?X⸮.
PAGE 36: 2F 71 AA C5 /q⸮⸮
PAGE 37: 26 2D A8 5D &-⸮]
PAGE 38: 2A D2 09 6D *⸮.m
PAGE 39: 81 D8 DD 89 ⸮⸮݉
PAGE 40: A7 B9 FF BB ⸮⸮⸮⸮
PAGE 41: 72 D2 AE DB rҮ⸮

So I can successfully transmit the integer I want 123456789, and I'm happy with that, but I'm not sure that this is how it would be done practically for my goal : Readout of external resistor value at about 100Hz.

I bought the NHS3152 chip because it is able in principle to transmit data at a datarate of 106 kb/s so I'd like to optimize my way of doing the readout.

So here are my questions, if someone can help :

1. Is wanting a 100 Hz readout possible using NDEF messages ? Because as I see from PAGE 00 to PAGE 41 there is a lot of "junk" information I don't need for my project. By the way I don't know how much time it takes for the 41 pages to be read, that would be a nice information to have.

2. Is there a smarter way to do that ? An int is supposed to be 4 bytes

3. (This is more a C/C++ question) I arbitrarily put 16 as the size of the char array : char str_adcInput[16]; and uint8_t payloadText[16]; This implies "junk" information after the "123456789" (it is quite random, for instance I read "1234567894???" on my phone using an Android NFC reader, the "4???" shouldn't be there).

What size should I put instead of 16 ? sizeof(int) or 4*sizeof(int) (or something else) ? (I know an int is 4 bytes but I don't know if we specify in bits of bytes)

Thank you for reading this post, any help is welcome !

Best,

Achraf

0 Kudos
Reply
1 Reply

1,063 Views
driesmoors
NXP Employee
NXP Employee

Hi,

The NDEF TLV starts at page 6:

T == 03h

L == 16h == 22 decimal.

So you can stop reading after 22 bytes. As an extra verification, you can check the terminator TLV right after the NDEF message (FEh on page 12).

To get rid of the noise after your integer, but before the terminator TLV, you can use strlen iso sizeof, so that only the 'stringified' number is copied, not the whole reserved buffer space.

Or, you can decide to not use NDEF messaging, or even not to use TLVs, but just dump it when ready. This has serious limitations, but

  • if your goal is to make it work as fast (and as soon) as possible
  • you are sure you control both sides at all times
  • you don't care about standard compliance
  • you are OK to potentially rewrite the communication part when the need arises:

just directly write a 32-bit word on a specific page, and read that page only from your Arduino. No need to turn it into a string, just write the numeric value.

On the NHS3152, that means bypassing the NDEFT2T module entirely. Just write your value 123456789 == 0x075BCD15 directly in the NFC shared memory to, say, page 42:

NSS_NFC->BUF[42] = 123456789;

(A slightly more sophisticated - still dedicated - approach is to look at the NFC shared memory as a circular buffer.)


Program your Arduino to read out a single page at 100 Hz, and have your NHS3152 firmware generate new numbers as fast as possible. A low-resolution conversion of the I2D takes 10 ms, one ADC conversion takes 12 us. You will not be able to generate them at 100 Hz on the NHS3152, but you can be close.

Aside: when you turn your attention to the actual sensing, also have a look at https://community.nxp.com/thread/486092

Best,
Dries.

0 Kudos
Reply