TagXplorer -support of ACR1281 reader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TagXplorer -support of ACR1281 reader

2,513件の閲覧回数
petrprachar
Contributor I

I would like to use TagXplorer windows desktop software with ACR1281 reader, but I get message "Reader not supported" when try to connect.

In the supported readers list this reader model is included. So I don't understand why I'm getting this message.

0 件の賞賛
11 返答(返信)

2,320件の閲覧回数
softzer0
Contributor II

Can anyone confirm that ACR 1281U-C1 works? Thanks!

0 件の賞賛

2,310件の閲覧回数
acesinvensys
Contributor I

No from my side 

0 件の賞賛

2,291件の閲覧回数
softzer0
Contributor II

I can confirm that C1 works, I've tested it right now.

0 件の賞賛

2,285件の閲覧回数
acesinvensys
Contributor I

Trued the library you mentioned, it was able to connect but on reading ntag213tt, tag not available 

 

 

0 件の賞賛

2,283件の閲覧回数
softzer0
Contributor II

I was testing it on NTAG 424 DNA chips.

0 件の賞賛

2,265件の閲覧回数
acesinvensys
Contributor I

Buddy do you have acr1281 sdk or any sample codes library you can share 

0 件の賞賛

2,258件の閲覧回数
softzer0
Contributor II

No, I don’t use that.

0 件の賞賛

2,350件の閲覧回数
acesinvensys
Contributor I

I am facing the same issue , ACR 1281U-C2 not supported , the tagXplorer is hardcoded for specific reader I guess.

 

0 件の賞賛

2,377件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Petr Prachar,

Please contact thecompany in charge of this ACR reader it might need a firmware update, since this is not an NXP reader is hard for me to tell whether this problem is related to TagXplorer. please confirm with the manufacturer of the reader.

Have a great day !

BR

Jonathan

0 件の賞賛

2,264件の閲覧回数
acesinvensys
Contributor I

Need some sample sdk codes for using the taplinx and writing ntag213TT messages. 

How to start with reading writing on desktop 

0 件の賞賛

2,358件の閲覧回数
softzer0
Contributor II

I'm having the same problem here.

I'm using ACR 1281U-C2.

0 件の賞賛