TagXplorer -support of ACR1281 reader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TagXplorer -support of ACR1281 reader

2,491 Views
petrprachar
Contributor I

I would like to use TagXplorer windows desktop software with ACR1281 reader, but I get message "Reader not supported" when try to connect.

In the supported readers list this reader model is included. So I don't understand why I'm getting this message.

0 Kudos
11 Replies

2,298 Views
softzer0
Contributor II

Can anyone confirm that ACR 1281U-C1 works? Thanks!

0 Kudos

2,288 Views
acesinvensys
Contributor I

No from my side 

0 Kudos

2,269 Views
softzer0
Contributor II

I can confirm that C1 works, I've tested it right now.

0 Kudos

2,263 Views
acesinvensys
Contributor I

Trued the library you mentioned, it was able to connect but on reading ntag213tt, tag not available 

 

 

0 Kudos

2,261 Views
softzer0
Contributor II

I was testing it on NTAG 424 DNA chips.

0 Kudos

2,243 Views
acesinvensys
Contributor I

Buddy do you have acr1281 sdk or any sample codes library you can share 

0 Kudos

2,236 Views
softzer0
Contributor II

No, I don’t use that.

0 Kudos

2,328 Views
acesinvensys
Contributor I

I am facing the same issue , ACR 1281U-C2 not supported , the tagXplorer is hardcoded for specific reader I guess.

 

0 Kudos

2,355 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Petr Prachar,

Please contact thecompany in charge of this ACR reader it might need a firmware update, since this is not an NXP reader is hard for me to tell whether this problem is related to TagXplorer. please confirm with the manufacturer of the reader.

Have a great day !

BR

Jonathan

0 Kudos

2,242 Views
acesinvensys
Contributor I

Need some sample sdk codes for using the taplinx and writing ntag213TT messages. 

How to start with reading writing on desktop 

0 Kudos

2,336 Views
softzer0
Contributor II

I'm having the same problem here.

I'm using ACR 1281U-C2.

0 Kudos