TagXplorer - ACR 1281U-C1 not listed in readers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TagXplorer - ACR 1281U-C1 not listed in readers

Jump to solution
2,348 Views
softzer0
Contributor II

I have the reader in the subject and I'm using Windows 10 with correctly installed drivers for it, as it can be seen in the attachment. When I open TagXplorer application, it says that no reader is connected. Can anyone tell me what should I do?

softzer0_0-1600257378443.png

 

0 Kudos
Reply
1 Solution
2,338 Views
softzer0
Contributor II

This is solved somehow by restarting the computer after installing drivers. This topic can be closed.

View solution in original post

0 Kudos
Reply
5 Replies
2,339 Views
softzer0
Contributor II

This is solved somehow by restarting the computer after installing drivers. This topic can be closed.

0 Kudos
Reply
2,331 Views
acesinvensys
Contributor I

If possible please share drivers 

0 Kudos
Reply
2,329 Views
softzer0
Contributor II

I have downloaded these and installed them manually: https://www.acs.com.hk/download-driver-unified/10903/ACS-Unified-Driver-Win-4300.zip

0 Kudos
Reply
2,333 Views
acesinvensys
Contributor I

Are you able to read tags using this reader. 

 

0 Kudos
Reply
2,326 Views
softzer0
Contributor II

Yes, I’m able to do everything.

0 Kudos
Reply