I have a recently purchased the NXP Pegoda 2 (CLRD710) and installed tagXplorer v1.2 (Build Version: 2019-02-14 175055) on a Windows 10 PC. The "NXP Pegoda 2 N 0" connects to tagXplorer, but I get "Reader is not supported.". See attached screenshots.
Please advise because according to NXP documentation, the Pegoda 2 reader is supported. Maybe I need a dedicated driver for the Pegoda?
解決済! 解決策の投稿を見る。
Vincent Coli, please check the quick start guide section 8, but basically first you will need to carefully (to avoid breaking the LED connections) open the PEGODA reader top then configure the DIP switch to the flash state
then connect it to the PC, open it as mass storage device and drag and drop the firmware files. for more explicit content please check the quick start guide in the link above and if you have more questions or issues let me know.
Have a great day !
BR
Jonathan
Jonathan,
That worked -- thanks!#
Jonathan,
Thank you for your help. I installed the Driver, but I am not able to update the firmware. Can you advise how to do this? I am running Windows 10. the QuicSstart refers to Windows 7.
As you can see, I can connect to the Pegoda Reader, but not the NTAG216 card. The Smartcard Utility reports I am running firmware 1.33.11. The link you provided lists current to be 2.2.8.
Thanks,
Vince
Vincent Coli, please check the quick start guide section 8, but basically first you will need to carefully (to avoid breaking the LED connections) open the PEGODA reader top then configure the DIP switch to the flash state
then connect it to the PC, open it as mass storage device and drag and drop the firmware files. for more explicit content please check the quick start guide in the link above and if you have more questions or issues let me know.
Have a great day !
BR
Jonathan
Dear Vincent Coli,
Please check you have the lates firmware version in the PEGODA reader you can found the latest firmware here please check the Quick startup guide to know how to flash the firmware. as you can see I was able to connect the PEGODA 710 and connect a tag
Have a great day !
BR
Jonathan