PN7462 nfc cockpit调试

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 nfc cockpit调试

1,071 Views
wkayingk
Contributor I

我在用PN7462板子和NFC cockpit软件调试我设计的一个标签(PICC)时,
参照的是iso14443-a的第三层协议,发现NFC cockpit软件在这里可以收到ATQA和SAK命令但无法显示PICC的UID,
标签设计时,UID配置为0x18,0x00,0x00,0x00(uid0~uid3),
ATQA设置为0x00,0x03
84e531a7bed8fa49f1573762ff55620.png

 

0 Kudos
Reply
2 Replies

1,044 Views
alice1
Contributor II

你好!您的问题解决了吗?我也遇到类似问题能不能分享一下解决方法

0 Kudos
Reply

1,053 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

 

不知道你是否曾经尝试直接在Data to be send发送命令,然后检查Card response中收到的数据,也是相同的结果吗?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply