PN7462 firmware with NFC Cockpit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 firmware with NFC Cockpit

1,079 Views
s_ali
Contributor III

Hi

We are trying to use PN7462 Development kit over VCOM USB interface with NFC Cockpit v4.8.0 but getting the following error:

pastedImage_1.png

Is the following the correct firmware for PN7462 to use with NFC Cockpit?

pastedImage_2.png

Thanks in advance

Labels (2)
0 Kudos
1 Reply

1,007 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

As I know, there is a issue with the latest Cockpit for PN7462EVB communication, please use 4.3 instead, and please also program PN7462EVB with the firmware in Cockpit 4.3.0 installation folder, e.g, C:\nxp\NxpNfcCockpit_v4.3.0.0\firmware\PN7462AU
Please refer to "6.8 Updating Flash and EEPROM via USB MSD interface" in UM10883 for more details.

Hope it help you. Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos