PN7160 SPI EVK (OM27160B1EVK) on Raspberry Pi4 : no NFC tag detected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7160 SPI EVK (OM27160B1EVK) on Raspberry Pi4 : no NFC tag detected

Jump to solution
11,659 Views
fr5
Contributor IV

Hi,

I followed instructions provided in these documents :
https://www.nxp.com/docs/en/application-note/AN12991.pdf
https://www.nxp.com/docs/en/application-note/AN13287.pdf
https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Easy-set-up-of-NFC-on-Raspberry-Pi/ta-p/1099... by @jeremygeslin 

I have tested with nfcDemoApp on two different configurations.

On first configuration I used a Raspberry yocto image with https://github.com/NXPNFCLinux/meta-nxp-nfc/blob/master/recipes-nfc/nxp_nfc/nxp-nfc_git.bb recipe, with SRC_URI overrided to git://github.com/NXPNFCLinux/linux_libnfc-nci.git;branch=NCI2.0_PN7160 and SRCREV to "6bf9f42b94e267f6384043009bda84c11e7ebbaa".

On second configuration I used directly Raspberry debian distribution (debian version 11.2) on which I installed linux_libnfc-nci library got from git clone https://github.com/NXPNFCLinux/linux_libnfc-nci.git -b NCI2.0_PN7160

In both cases I am not able to detect a NFC tag (I attach the corresponding log files).

Can anyone help on this please ?

Regards,

Fabien

Labels (1)
0 Kudos
1 Solution
11,614 Views
jeremygeslin
NXP Employee
NXP Employee

Hi Fabien,

From your logs, I can observe the discovery loop is started with the following NCI command:

21031309000101010201030180018101060174017701

This RF_DISCOVER_CMD is rejected by PN7160 with SYNTAX_ERROR:

41030105

 

FYI, the command detail is:

[NCI][COMMAND][21 03 13 09 00 01 01 01 02 01 03 01 80 01 81 01 06 01 74 01 77 01]
   RF_DISCOVER_CMD
      * Number of Configurations = 9 [0x09]
         --> Configuration N° 1
            - RF Technology and Mode = {Std} NFC_A_PASSIVE_POLL_MODE [0x00]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

         --> Configuration N° 2
            - RF Technology and Mode = {Std} NFC_B_PASSIVE_POLL_MODE [0x01]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

         --> Configuration N° 3
            - RF Technology and Mode = {Std} NFC_F_PASSIVE_POLL_MODE [0x02]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

         --> Configuration N° 4
            - RF Technology and Mode = {Std} NFC_A_ACTIVE_POLL_MODE (RFU) [0x03]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

         --> Configuration N° 5
            - RF Technology and Mode = {Std} NFC_A_PASSIVE_LISTEN_MODE [0x80]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

         --> Configuration N° 6
            - RF Technology and Mode = {Std} NFC_B_PASSIVE_LISTEN_MODE [0x81]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

         --> Configuration N° 7
            - RF Technology and Mode = {Std} NFC_15693_PASSIVE_POLL_MODE (RFU) [0x06]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

         --> Configuration N° 8
            - RF Technology and Mode = Reserved for Proprietary Technologies in Poll Mode [0x74]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

         --> Configuration N° 9
            - RF Technology and Mode = Reserved for Proprietary Technologies in Poll Mode [0x77]
            - Discovery Frequency    = RF Technology and Mode will be executed in every discovery period [0x01]

 

The "RF Technology and Mode" value 0x77 relates to KOVIO, as defined for PN7150, while it should be 0x70 for PN7160. We are currently analyzing why the proper value is not internally used by the libnfc-nci, but nevertheless disabling KOVIO from POLLING_TECH_MASK should remove the related configuration in the RF_DISCOVER_CMD.

 

Thus can you please verify the configuration files located under /usr/local/etc/, since those are the one dynamically loaded during libnfc-nci initialization (there are copied there during "make install" operation).

 

Regards,

Jeremy.

 

 

 

View solution in original post

24 Replies
937 Views
MJY
Contributor I

This patch can only fix the poll mode; other modes are still facing the same error

0 Kudos
169 Views
MJY
Contributor I

It worked; I forgot to run 'make install'

0 Kudos
170 Views
andraz_skupek
NXP Employee
NXP Employee

Hi,

can you please send the error message?

 

Best regards,

Andraz

0 Kudos
2,665 Views
steve_delahunty
Contributor II

Yes, this patch will fix the issue. Good luck!

 

0 Kudos