PN7150 emc filter desing without balun

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 emc filter desing without balun

1,706 Views
alikarakaş
Contributor I

How can i desing pn7150 emc filter with triax coax? Maximum length for triax cable 20cm. Can ve desing without balun .

Labels (1)
0 Kudos
Reply
4 Replies

1,590 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear ali ,

   See suggestions below, please!

1. Design your matching circuit and EMC circuit according to the 50 ohm antenna solution.

2. Reserve RXN for RX balun

In this way, the signal can be received either single-ended or differential.

Solutions for 50OHM single-ended solution will sent to your email. Pay attention to checking it, please!

Have a nice day!

BR,

NXP TIC Weidong

0 Kudos
Reply

1,590 Views
alikarakaş
Contributor I

Thank is for your reply. But im connecting tvss line to gnd directly. İs correct for short range antenna ? .

iPhone’umdan gönderildi

Wigros Sun <admin@community.nxp.com<mailto:admin@community.nxp.com>> şunları yazdı (29 Nis 2019 04:30):

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

You have been mentioned

by Wigros Sun<https://community.nxp.com/people/weidong.sun?et=notification.mention> in Re: PN7150 emc filter desing without balun in NXP Community - View Wigros Sun's reference to you<https://community.nxp.com/message/1144808?commentID=1144808&et=notification.mention#comment-1144808>

0 Kudos
Reply

1,590 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear ali,

   >> But im connecting tvss line to gnd directly. İs correct for short range antenna ?

VSS(TX) pin should be connected to GND, so you are right.

[comment)

  VSS(TX) on PN7150 is TVSS.

Have a nice day!

Best regards,

NXP TIC Weidong Sun

0 Kudos
Reply

1,479 Views
erichwolf
Contributor I

Hello Weidong Sun,

please can you post the single ended Antena design in the forum or send it by email?

Thank you

 

 

0 Kudos
Reply