Hello,
I'd like to communicate very fast from a PN532 (PICC) device with a PN512 (PCD) Initiator using the ISO14443-4. I have a lot of data to transfer from PICC to PCD. Since the PN512 has only 64 bytes in the FIFO, the PN532 uses the chaining mode to transfer 256 bytes. I use the command 0x8E in PN532 to send 256 bytes and I can see that there're 4 x 64-bytes transmitted from PN532 to PN512.
I attached an image to show the first 64 bytes transmission.
I'd like to understand why it takes several ms for the PN532 to transmit the first 64 bytes. Is there a way to improve that? To reduce the process time to send the first packet?
Please, refer to the image to understand my issue. I took several days before posting this message.
Thank you very much!
Hello,
I did a small mistake in the picture. It takes 9.9 ms to receive (PCD) the first packet. At 424 kbits per seconds, a 64 bytes should take around ~1.5 ms, but why does the PN532 take 9 ms to send the first packet and also the next ones. The PN532 firmware version is 1.6.
I attach a new picture...
Hi Christian,
Would you please provide more details on the setup regarding PN532 and PN512? Thanks for your patience!
Have a great day,
Kan
Hello Mr Kan,
Sorry for this very very long delay. I was busy on a new project and now, I come back to this issue. It's really not fixed. I would like to transfer data as fast as possible but I noticed that the PN532 device sends very slow the data. What information do you need to understand more the problem?
I use the PN512 to receive the data and I noticed that it takes more than 10 ms to receive the first 64 bytes packet. It's too slow when I initialized the speed to 424 kbps.