PN5180 BGA signal definitions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 BGA signal definitions

1,100 Views
izmile
Contributor III

Hello all,

Has anyone used PN5180 in BGA package? I have got the pinouts for the package (under NDA) but there seems to be couple of signals which do not have proper definitions. 

 

Signal #1: PRD

Signal #2 : TVDD_IN    

- Note that there is already a TVDD pin in the package. I am not sure what TVDD_IN is for. Further, TVDD and TVDD_IN are not connected inside the package.

 

Any ideas on what these signals are used for?  

I have raised a support question with NXP.. but they have gone quiet.. :-(

Thanks,

-Ismail

2 Replies

926 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Mohamed,

    You can float these 2 signals on your deisgn!  no any effect for your solution.

Best Regards,

Weidong

0 Kudos
Reply

926 Views
izmile
Contributor III

Hi Sun,

Thanks for the reply. 

Just curious, what are these signals for? Full signal definitions would be very helpful.

Thanks,

-Ismail