Hello,
But, I'm using the FRDM-K64F.
Thanks!
Hi ,
Please kindly refer to the nfcDemoApp from OM5578-PN7150S_Rpi_Linux_demo_v1.1.zip - Box , its write mode can be used for Mifare Classic.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kan,
I am also using K64f and trying to write data to MIFARE classic cards with the help of OM 5578/PN 7150. Is it possible?
Thanks,
Shruti
Yes. There is an example for FRDM-K64F, please kindly refer to NXP-NCI Kinetis Design Studio example for details.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------