OM27160A1EVK/PN7160 Not Detected, Demo App Fails With "NfcService Init Failed"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM27160A1EVK/PN7160 Not Detected, Demo App Fails With "NfcService Init Failed"

1,311 Views
shoulihan
Contributor II

Hello, 

We recently purchased a few OM27160A1EVK development kits. We are testing with the raspberry pi interface board and a Raspberry Pi 3b+ with a fresh install of Raspbian on it. We have followed the quickstart documentation, however, the demo application fails with "NfcService Init Failed Leaving...". Additionally, the Pi is unable to detect the device via i2c. "sudo i2cdetect -y -a -r 1" fails to display any device. "sudo i2cdump 1 0x28" also fails to work. We have also tried other devices, such as a Jetson Nano, as well as multiple development kits. No combination is able to be detected. 

0 Kudos
Reply
6 Replies

530 Views
Caputo
Contributor I

Hello Daniele,

I too am experiencing the same issue, despite having followed the documentation step by step. I noticed that the documentation references the following two interfaces: OM27160B1EVK, OM27160A1EVK

The one I have is: OM27160A1HN Are there any configuration differences for this model? Please, if there are any solutions, could I be informed? Thank you.

0 Kudos
Reply

504 Views
Tomas_Parizek
NXP Employee
NXP Employee

Hello Caputo, 

 

See this case -> https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825250/thread-id/...

 

about the PN7160 versions:

A1 -> I2C 

B1-> SPI 

 

BR

Tomas 

0 Kudos
Reply

1,285 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @shoulihan 

 

I would suggest you refer to below link: Easy set-up of NFC on Raspberry Pi

https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Easy-set-up-of-NFC-on-Raspberry-Pi/ta-p/1099...

Though it is for PN7150,  it should be very similar to PN7160

 

Regards

Daniel

0 Kudos
Reply

1,238 Views
shoulihan
Contributor II

Hello, we would really appreciate any help any community member or NXP employee can provide. The quickstart guide is quite brief and simple, and the fact that it can't be followed on numerous OM27160A1EVKs, Raspberry Pis, etc. is worrying.  

0 Kudos
Reply

1,145 Views
danielchen
NXP TechSupport
NXP TechSupport

Sorry,  did you solved this issue?  I suggest you check the configuration file.  I have rasperberry pi 4 board  that works well with PN7160.   could you please send me your configure file ?

 

Regards

Daniel

0 Kudos
Reply

1,272 Views
shoulihan
Contributor II

Hello Daniel,

We appreciate your response. The instructions you linked appear to be an older (outdated) version of the instructions from the quickstart guide (https://www.nxp.com/docs/en/application-note/AN12991.pdf). We have followed these instructions (for working with a Raspberry pi via i2c) from start to finish numerous times with various hosts, development kits, fresh installs of Raspbian, etc., and cannot get the demo app to work as shown in the guide. In our opinion, the fact the device is not detectable by the Raspberry Pi via i2cdetect or any other i2c utility makes it seem that there could be a deeper issue. From the documentation, we expect to see the device on i2c-1 at address 0x28, which is not the case. 

0 Kudos
Reply