Hi Ivan, Sir,
I read the examples and study some documents.
Now I can read/write the register of the sensor by calling the I2C API funciton "Chip_I2C_MasterCmdRead"/"Chip_I2C_MasterSend" respectively.
But the problem I met is that I canNOT operate the I2C by calling the API functions above repeatedly.
My test items/steps are:
1. send data to I2C slave to get the register data of the sensor by call "Chip_I2C_MasterCmdRead";
2. send data to I2C slave to write the register of the sensor by call "Chip_I2C_MasterSend";
3. send data to I2C slave to get the register data of the sensor again by call "Chip_I2C_MasterCmdRead";
If I just have only item 1 (or 2, or 3) to test, it is ok for the correct operation and result.
But when I have the three items to test together, it is failed to operate the item 2 and item 3 for the results.
The API function never return for item 2 and item 3.
And here are the code snippets based on "app_example_dp_i2c" to test:
------
// for test item 1. send data to I2C slave to get the register data of the sensor by call "Chip_I2C_MasterCmdRead";
static void Slave0Access(void)
{
uint8_t slaveAddr = 0x19;
uint8_t regAddr = 0x20; // 0x0F;
uint8_t readData = 0;
// printf("Slave0Access\r\n");
Chip_I2C_MasterCmdRead(I2C0, slaveAddr, (uint8_t *)®Addr, (uint8_t *)&readData, 1);
// printf("Read slaveAddr 0x%02X, regAddr 0x%02X, readData 0x%02X\n\r", slaveAddr, regAddr, readData);
}
// for test item 2. send data to I2C slave to write the register of the sensor by call "Chip_I2C_MasterSend";
static void Slave1Access(void)
{
uint8_t slaveAddr = 0x19;
uint8_t regAddr = 0x20;
uint8_t writeData = 0x57;
uint8_t txBuf[2] = {0x00};
// printf("Slave1Access\r\n");
txBuf[0] = regAddr;
txBuf[1] = writeData;
Chip_I2C_MasterSend(I2C0, slaveAddr,txBuf, 2);
// printf("Write slaveAddr 0x%02X, regAddr 0x%02X, writeData 0x%02X\n\r", slaveAddr, regAddr, writeData);
}
// for test item 3. send data to I2C slave to get the register data of the sensor again by call "Chip_I2C_MasterCmdRead";
static void Slave2Access(void)
{
uint8_t slaveAddr = 0x19;
uint8_t regAddr = 0x20;
uint8_t readData = 0;
// printf("Slave2Access\r\n");
Chip_I2C_MasterCmdRead(I2C0, slaveAddr, (uint8_t*)®Addr, (uint8_t*)&readData, 1);
// printf("Read slaveAddr 0x%02X, regAddr 0x%02X, readData 0x%02X\n\r", slaveAddr, regAddr, readData);
}
// here is the calling for test 1, 2, 3:
void Master_PollSlaves(void)
{
// printf("Master_PollSlaves\n\r");
/** Device Id Use Case*/
Slave0Access();
/** Temperature Use Case */
Slave1Access();
/** LED Use Case */
Slave2Access();
/** Scratchpad/Counter Use Case */
// Slave3Access();
// Chip_Clock_System_BusyWait_ms(I2C_MASTER_COMM_INTERVAL);
}
------
It is very appreciated if anyone can help me to review if anything wrong.
And any limitation to use the I2C API?
Thanks,
Arna