Hi,
I need your help !
I installed 2 version of NFC cockpit in the past (and 2 weeks ago everithing worked fine)
But today when I wanted to start NFC cockpit 0.5.8 nothing happen .
I can see the process in the windows task manager (details) but no interface or icon in taskbar appeared !
I tried to uninstall the 2 versions then reboot and install the last one 0.5.9 but same result .
I also tried to execute it with windows in safe mode but problem still the same.
I installed it on my colleague's laptop and it works.
Do you have an idea to solve my issue ?
Best regards
Nicolas
Hello Nicolas,
Thank you for using our NXP products we really appreciate the preference,
This might indicate that the problem isn't a software problem but a Windows issue.
Could it be possible that another program might be interfering with the correct initialization of NFC Cockpit? Maybe an afterward installed program.
Probably yes, but which one? I tried to remove latest programs installed without success.
Do you know some programs that can generate this kind of issue?
Nobody have a suggestion ?
I tried to reinstall .net SDK, runtime and also microsof windows desktop runtime .... , but problem still here and only with NFC_Cockpit.
herewith copy of log file :
[2021.06.01 10:42:20]:DEBUG :ServiceBroker :ReadWriteNotify registration successfull
[2021.06.01 10:42:21]:ERROR :App :Internal Error occured "The invocation of the constructor on type 'NFCInfraSupportTool.ViewModels.BoardConnectionViewModel' that matches the specified binding constraints threw an exception." in PresentationFramework
[2021.06.01 10:42:21]:DEBUG :App :Error location" at System.Windows.Markup.WpfXamlLoader.Load(XamlReader xamlReader, IXamlObjectWriterFactory writerFactory, Boolean skipJournaledProperties, Object rootObject, XamlObjectWriterSettings settings, Uri baseUri)
at System.Windows.Markup.WpfXamlLoader.LoadBaml(XamlReader xamlReader, Boolean skipJournaledProperties, Object rootObject, XamlAccessLevel accessLevel, Uri baseUri)
at System.Windows.Markup.XamlReader.LoadBaml(Stream stream, ParserContext parserContext, Object parent, Boolean closeStream)
at System.Windows.Application.LoadBamlStreamWithSyncInfo(Stream stream, ParserContext pc)
at System.Windows.Application.LoadComponent(Uri resourceLocator, Boolean bSkipJournaledProperties)
at System.Windows.Application.DoStartup()
at System.Windows.Application.<.ctor>b__1_0(Object unused)
at System.Windows.Threading.ExceptionWrapper.InternalRealCall(Delegate callback, Object args, Int32 numArgs)
at System.Windows.Threading.ExceptionWrapper.TryCatchWhen(Object source, Delegate callback, Object args, Int32 numArgs, Delegate catchHandler)"