NFC NTAG NT3H1101 pass-through SRAM issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC NTAG NT3H1101 pass-through SRAM issues

870件の閲覧回数
martinbirkebaek
Contributor I

I want to transfer data via NFC to a microcontroller via the pass-through interface. I have it working so that i am able to transmit data from a windows application to the microcontroller via NFC reader/writter. But when I try to respond from the microcontroller, my writes to SRAM fails. I can address the NFC chip via I2C, but as soon as i transmit the first byte, it gets nak'ed by the NFC chip and i do not understand why. NS REG reads 0x65.

タグ(1)
0 件の賞賛
4 返答(返信)

677件の閲覧回数
chengwei_gao112
Contributor I

I meet the same problem with you,do you solve it now? I care for it very much ! My email is154824072@qq.com

0 件の賞賛

677件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Martin,

Was the tag VCC powered?


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

677件の閲覧回数
sunxin
Contributor II

I meet the same problem with you,do you solve it now? I care for it very much ! My email is 1015902665@qq.com

0 件の賞賛

677件の閲覧回数
martinbirkebaek
Contributor I

Hi Kan,

Yes VCC is powered.

best regards,

Martin

0 件の賞賛