NFC Electromagnetic Compatibility for CE compliance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Electromagnetic Compatibility for CE compliance

1,633件の閲覧回数
fourtrax
Contributor I

Hi, I am using a PN532 and experiencing the problem that energy is magnetically coupled from the NFC antenna into the power cords that are connected to my device.

I did a precompliance measurement using a spectrum analyser and a DC-LISN that shows values above the 1mV limit for 13.56 Mhz (no harmonics or anything else).

Unfortunately I can not move the connector further away from the antenna on the pcb, also attempts to shield it using a ferrite sheet didn't help much. Twisting the power cable reduces the peak but I can not rely on that being done by the user.

Will the 13.56 Mhz peak make me fail the EMC conducted emission test or are there any exceptions for NFC regarding conducted (and radiated) emissions ?

thanks in advance

0 件の賞賛
返信
1 返信

1,366件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Gerrit,

   About CE certification of PN532, you can contact mobile team of local NXP.

Best regards,

Weidong Sun

0 件の賞賛
返信