My New OM27462CDKP not connecting to NFC Cockpit (VCOM not appearing)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

My New OM27462CDKP not connecting to NFC Cockpit (VCOM not appearing)

115 Views
Mahmoud_Awad
Contributor I
Hello, I'm connecting my new OM27462CDKP through the micro-USB cable (with default jumper settings). the board is powered up but no VCOM port appears in the device manager and NXP NFC Cockpit isn't detecting any Ports or connected Boards. PS: the VCOM files are already installed in the NFC Cockpit's path and the installation of NFC Cockpit was run as administrator and didn't face any issues during installation.
0 Kudos
2 Replies

77 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi 

 

This seems a driver issue.  You can check whether the USB port works normally,  reinstall the driver  , or change a new USB cable.

 

Regards

Daniel.

0 Kudos

54 Views
Mahmoud_Awad
Contributor I

I found the solution, I had to enter the mass storage mode and update the EEPROM and Flash firmware binaries after that the VCOM appeared and NFC Cockpit recognized the board.

Thanks.

Tags (1)
0 Kudos