Hi All,
I am using #MIFARE DESFire Light for one of my customer. I can successfully authenticate the card using DESFireEV2First algorithm. After that I'm trying to get the session keys (SesAuthENCKey/SesAuthMACKey) as explained in example of AN12343, Chapter 7.1.3.1/7.1.4, but I can not get the expected output for the session keys.
So, my concern is, Can I use same CMAC algorithm in DESFire Light which was worked in DESFire EV1?
If YES, output of CMAC algorithm used in DESFire EV1 = 8 bytes (MAC)
And we want output of CMAC algorithm in DESFire Light = 16 bytes Session keys (SesAuthENCKey/SesAuthMACKey).
it looks confusing for me.
Any guideline regards this will be highly appreciable!
Hi Ivan,
Thanks for the response. The issue was with the XOR calculation. Now, I can get the correct Session keys from the active DESFireEV2 first authentication of DESFire Light.
I’m facing issue in write data and read data after this.
1) When I try to WriteData in 00EF or 04EF, it gives me error 0x7E (LENGTH_ERROR).
I can successfully write data "22222222222222222222222222222222222222222222222222" in encrypted mode same as example of AN12343 (section 8.1.3).
But if I try to write my data which is 16 bytes or less i.e. "3132333435", it gives me 0x7E error.
>> Write Procedure I followed:
IV_Input = A55AFBCF7BCF00000000000000000000 (lable + TI + CmdCounter + Padding followed by 00)
SesAuthENCKey = 1D8C929597A19990295306DEFC57755A
IV = 00000000000000000000000000000000
IV_For Command Data = 6034C0FA74F032CBFFED3B6F3E9C584A
Data with Padding = 31323334358000000000000000000000
Encrypted Data = 77A2FD1B2BC19EC917B26D17694B6844
Command Header = 00000000050000
MAC_Input = 8D0000FBCF7BCF0000000005000077A2FD1B2BC19EC917B26D17694B6844
IV = 00000000000000000000000000000000
SesAuthMACKey = 2D9377F5CAAA1D53935454806B170723
Calculated MAC = CD3177470834C634
APDU to Card = 908D00001F0000000005000077A2FD1B2BC19EC917B26D17694B6844CD3177470834C63400
Response from Card = 917E (LENGTH_ERROR)
Can you guide me which one is the wrong step I'm followed.?
2) Also, I have followed below steps to read data 22222222222222222222222222222222222222222222222222”,
but it gives me 0x1E (INTEGRITY_ERROR).
>> Read Procedure I followed:
IV = 00000000000000000000000000000000
Command Header = 00000000190000 (FileID = 00, offset = 000000, DataSizeToRead = 19 bytes)
MAC_Input = AD0100B39DB01400000000190000
MACKey = C3D79B25473D4DC735F856F6DA8F7C22
Calculated MAC = E2B5F6406CF1FA8C
APDU to Card = 90AD00000F00000000190000E2B5F6406CF1FA8C00
Response from Card = 911E (INTEGRITY_ERROR)
Can you guide me which one is the wrong step in read data I'm followed.?
NFC
Hello,
I'm currently working on generating the session keys for MIFARE DESFire Light. Is there a library you used to generate the CMAC algorithm? I've tried multiple solutions but I'm unable to generate the proper values.
Thank you!