Hi Everyone,
I am using NFC Cockpit v5.8.0 with PNEV7462C. I tried the LPCD function but it always reported "Card/Load detected in the field" even if there is no card/tag. I am not sure the reason. Any idea?
Thanks,
Chris
Hello @ChrisPark ,
The LPCD should only be used with disabled DPC. Did you disable DPC ? Please kindly refer to https://www.nxp.com/docs/en/application-note/AN11785.pdf for more details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kan,
Thank you for your reply. I have disabled DPC by writing 0xF2 to DPC_CONTROL as below:
INFO:EEPROMService_PN7462AU:Write to EE address:0x201352. Value=0xF2
INFO:EEPROMService_PN7462AU:Read from EE address:0x201352. Value=0xF2
What did I miss yet?
Thanks,
Chris
Hi @Kan_Li,
According to AN11742, it mentions a Rx resistor (e.g. on page 12). However, I cannot find the resistor on the board PNEV7462C. Could you please give me a hint?
Thaks,
Chris
Hi @ChrisPark ,
They are R2a and R7a, please kindly refer to UM10883 for more details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------