compre un kit PN7120 NFC Controller SBC kit OM5577/PN7120S pero baje el sistema operativo OM5577-PN7120S_Win10IoT_demo_v1.0.zip pero al descomprimir ocupa mas memoria que la que recomiendan de 4 GB, pregunta: requiero instalar en una memoria de 8 Gb o hay una version de OS mas pequeña?
no i mean downloaded windows 10 from nxp but in a video it says in a 4 Gb memory can put the image but even in a 8gb memoriy there is no enough memory so used a 16 gb memory but when i try to star the RPi2 with W10 sends an error about PNP_DETECTED_FATAL_ERROR so i don't know i to start again installing one more time the SO W10 in the memory
so you can put the image to the SD card and then boot up the board from the SD card.