In the NXP's website , i only can fond the overview about P5CD012 , but i can't find the application note about it.
Who can provide me some information about how to operate it.
Thank you a lot!
1.1 CMOS14 SmartMX family features overview
The CMOS14 SmartMX family members are a modular set of devices featuring:
Hi - besides the comments from Kan_Li, also note that this is an older platform of NXP secure microprocessors. SmartMX P5 devices were actively sold between 2004 and 2013. Since then, a successor product family (SmartMX2 P60) has been available. Today, we are selling the second successor product family - SmartMX3 P71D321.
If you are selecting a secure microprocessor product, it is suggested to use the newest platform possible; this is for security but also for performance reasons.
Hi,
You need to sign NDA and register into NXP Docstore to access all documentation and sample code. You may contact your local sales or DFAE for help with it. Please refer to the following links for more details.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------