Has NXP announced an End-of-Life date for the CLRC663? Is the CLR663 still "Recommended for new designs"?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has NXP announced an End-of-Life date for the CLRC663? Is the CLR663 still "Recommended for new designs"?

ソリューションへジャンプ
1,339件の閲覧回数
vincentcoli
Contributor II

We are starting a new design which is based on the CLRC663.  We want to know the expected supply life if we stay with the CLRC663.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,098件の閲覧回数
michaelneurohr
NXP Employee
NXP Employee

Dear Vincent Coli,

The CLRC663 is a product which is sold in high volumes and there are no plans to discontinue this product.

Regards,

Michael

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,099件の閲覧回数
michaelneurohr
NXP Employee
NXP Employee

Dear Vincent Coli,

The CLRC663 is a product which is sold in high volumes and there are no plans to discontinue this product.

Regards,

Michael

0 件の賞賛
返信