For MFRC531 to read the serial number from a 14443B card, is sending “File read” APDU command sequence (File ID is - FE, 14) as { 0x00, 0xA4, 0x08, 0x00, 0x02, 0xFE, 0x14, 0x00} correct?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For MFRC531 to read the serial number from a 14443B card, is sending “File read” APDU command sequence (File ID is - FE, 14) as { 0x00, 0xA4, 0x08, 0x00, 0x02, 0xFE, 0x14, 0x00} correct?

732件の閲覧回数
greg_turner
Contributor I

For MFRC531 to read the serial number from a 14443B card, is sending “File read” APDU command sequence (File ID is - FE, 14) as { 0x00, 0xA4, 0x08, 0x00, 0x02, 0xFE, 0x14, 0x00} correct?  Trying to implement additional card type support on existing code.

ラベル(1)
0 件の賞賛
返信
1 返信

593件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

As I know, 0x00, 0xA4 is "Select File" command.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信