Hi All,
I have a couple of questions regarding PN7462 with 160KB.
I want to use PN7462 with TCP/IP and an RTOS if needed.
1. Do I need to use an RTOS to make use of TCP/IP on integrated Cortex M0 ?
2. If I need an RTOS, do I need extra storage space or flash on board to support this. How much ?
Thanks,
Gun
Hi Gun,
Actually you don't have to worry about the RTOS, PN7462AUPspPackageFull-v04_05_00 already included FreeRTOS in the package, you may directly invoke the system API from the library.Please kindly refer to the following for details.
for the above example, the total image size can be referred as below:
There should be enough space left for the your application code.
Please also note PN7462 doesn't contain an embedded Ethernet module, you have to use an external module which can be connected with SPI or I2C port.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kan,
Thanks for the answer. It does address the storage and RTOS questions.
I am not sure I should open another question but the followup question for me is if I add Ethernet or GSM module, should I write the "driver" myself ? In the case of GSM module, I can send AT command via serial or I2C and it should probably be ok.
Thanks,
Gun
Hi Gun,
Usually, the vendor of the Ethernet or GSM module would provide the driver/example for their products, so what you have to do at first is making sure the vendor has provided what you need , not only the hardware.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I think it should be porting the module driver to PN7462 project.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------