Hy,
I can´t get the NXP-NCI_LPC11xx_example working with the lpc1114 board and the OM5578 module.
I connected the pins as showen in AN11658.
The problem is that the I2C communication doesen´t work.
The log shows allways:
Running the NXP-NCI project.
Error: cannot connect to NXPNCI device
Any ideas what could be the problem?
Thanks
David
已解决! 转到解答。
Hi David,
Would you please check the following hardware settings?
- PN71xx VEN pin is not properly connected: it should be connected to LPC PIO3.5 which is LPCXpresson connector pin #47 (pay attention that the LPC1114a silkscreen is wrong, indicating P2.5 instead of P3.5). The VEN pin must be high to allow PN71xx operates.
- PN71xx IRQ pin is not properly connected: it should be connected to LPC PIO3.4 which is LPCXpresson connector pin #46 (pay attention that the LPC1114a silkscreen is wrong, indicating P2.4 instead of P3.4).
- the I2C lines are not pulled-up: LPC11xx doesn't offer internal pull-up setting of the I2C lines so external pull-up resistors must be added.
Please also check the optimization parameter in your project settings, please set it to "-O0" as below:
Please kindly let me know if the problem is still there.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi David,
Would you please check the following hardware settings?
- PN71xx VEN pin is not properly connected: it should be connected to LPC PIO3.5 which is LPCXpresson connector pin #47 (pay attention that the LPC1114a silkscreen is wrong, indicating P2.5 instead of P3.5). The VEN pin must be high to allow PN71xx operates.
- PN71xx IRQ pin is not properly connected: it should be connected to LPC PIO3.4 which is LPCXpresson connector pin #46 (pay attention that the LPC1114a silkscreen is wrong, indicating P2.4 instead of P3.4).
- the I2C lines are not pulled-up: LPC11xx doesn't offer internal pull-up setting of the I2C lines so external pull-up resistors must be added.
Please also check the optimization parameter in your project settings, please set it to "-O0" as below:
Please kindly let me know if the problem is still there.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------