After the PN7160 RF on, there are a large number of clutter signals in the IRQ and IIC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

After the PN7160 RF on, there are a large number of clutter signals in the IRQ and IIC

159件の閲覧回数
ethan_dang1
Contributor III

I'm testing with IMX6ULL+PN7160_EVK.

At first, the initialization and parameter configuration are normal, But when I send the RF_DISCOVER_CMD to PN7160, there is a lot of clutter on the IRQ pin, and there are some on the IIC pin as well. It is also not possible to check the card properly. When the VBAT_5V is removed, the clutter signal disappears.

I've tried using an external power supply to power VBAT and VDD_UP, but the phenomenon is the same.

Please help check.

0 件の賞賛
返信
3 返答(返信)

134件の閲覧回数
KellyLi
NXP TechSupport
NXP TechSupport

Hello @ethan_dang1 

Could you share the following information:

1) How to connect PN7160 and IMX6ULL?

2) Please provide demsg log

3) Please provide .dts file

BR

kelly

0 件の賞賛
返信

121件の閲覧回数
ethan_dang1
Contributor III

Hi Kelly,

Uploaded to attachments. Thanks!

0 件の賞賛
返信

98件の閲覧回数
KellyLi
NXP TechSupport
NXP TechSupport

Hello @ethan_dang1 

Could you switch to I2C2? Some sensors mounted on I2C1 may cause interference.

KellyLi_0-1717057697406.png

 

 

BR

kelly

0 件の賞賛
返信