After the PN7160 RF on, there are a large number of clutter signals in the IRQ and IIC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

After the PN7160 RF on, there are a large number of clutter signals in the IRQ and IIC

157 Views
ethan_dang1
Contributor III

I'm testing with IMX6ULL+PN7160_EVK.

At first, the initialization and parameter configuration are normal, But when I send the RF_DISCOVER_CMD to PN7160, there is a lot of clutter on the IRQ pin, and there are some on the IIC pin as well. It is also not possible to check the card properly. When the VBAT_5V is removed, the clutter signal disappears.

I've tried using an external power supply to power VBAT and VDD_UP, but the phenomenon is the same.

Please help check.

0 Kudos
Reply
3 Replies

132 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @ethan_dang1 

Could you share the following information:

1) How to connect PN7160 and IMX6ULL?

2) Please provide demsg log

3) Please provide .dts file

BR

kelly

0 Kudos
Reply

119 Views
ethan_dang1
Contributor III

Hi Kelly,

Uploaded to attachments. Thanks!

0 Kudos
Reply

96 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @ethan_dang1 

Could you switch to I2C2? Some sensors mounted on I2C1 may cause interference.

KellyLi_0-1717057697406.png

 

 

BR

kelly

0 Kudos
Reply