About LPCD function of MFRC6303

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About LPCD function of MFRC6303

875件の閲覧回数
1604204874
Contributor II

 I have doubt when use the function of RC6303 LPCD mode.As shown below,can you help me translate these few lines of assembly code into C language, I can't understand the assembly.Thanks!

pastedImage_1.png

ラベル(1)
0 件の賞賛
3 返答(返信)

634件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

I am sorry, but is the assembly code released by NXP? I need to find where it is from to get the right person to check it. Please kindly clarify.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

634件の閲覧回数
1604204874
Contributor II

Hello, NXP did not release the assembly code, but instead saw it in the application note AN11145 they released.

0 件の賞賛

634件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Binshen,

It is not assembly code, it is a script file for CLRC663 red board, for the related C file, there is an example , please refer to RC52xPcSerial Command explanation for details.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛