Is the SLRC61003 compatible with the CLEV6630 firmware?

cancel
Showing results for 
Search instead for 
Did you mean: 

Is the SLRC61003 compatible with the CLEV6630 firmware?

283 Views
thomas_haugen
Contributor I

Hi,

I am using the CLEV6630 NCF kit to communicate with a SLRC61003 chip. Done some modifications of cource and connected the kit with my board.

The NXP Cockpit will not communicate with it (expecting a CLRC663 Plus ?).

Regards Thomas

0 Kudos
1 Reply

221 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport


Hi

RC610 is the same core like RC663 -> so all SW must work the same way. Only difference: The EEPROM LUT (for toe load protocol) are different!and of course RC663 can do all protocols, RC610 can only do I-Code

 

 so both have same core but one support more protocols.

BR

Jonathan

0 Kudos