I have doubt when use the function of RC6303 LPCD mode.As shown below,can you help me translate these few lines of assembly code into C language, I can't understand the assembly.Thanks!
I am sorry, but is the assembly code released by NXP? I need to find where it is from to get the right person to check it. Please kindly clarify.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Binshen,
It is not assembly code, it is a script file for CLRC663 red board, for the related C file, there is an example , please refer to RC52xPcSerial Command explanation for details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------