static const uint16_t PH_MEMLOC_CONST_ROM wRc663_DefaultShadow_I14443b[][2] =
{
{PHHAL_HW_CONFIG_PARITY, PH_OFF},
{PHHAL_HW_CONFIG_TXCRC, PH_ON},
{PHHAL_HW_CONFIG_RXCRC, PH_ON},
{PHHAL_HW_CONFIG_RXDEAFBITS, 0x0008},
{PHHAL_HW_CONFIG_TXWAIT_US, 85},
#if 0
{PHHAL_HW_CONFIG_TXDATARATE, PHHAL_HW_RF_DATARATE_106},
{PHHAL_HW_CONFIG_RXDATARATE, PHHAL_HW_RF_DATARATE_106},
#else
{PHHAL_HW_CONFIG_TXDATARATE, PHHAL_HW_RF_DATARATE_424},
{PHHAL_HW_CONFIG_RXDATARATE, PHHAL_HW_RF_DATARATE_424},
#endif
{PHHAL_HW_CONFIG_TIMEOUT_VALUE_US, PHHAL_HW_RC663_DEFAULT_TIMEOUT},
{PHHAL_HW_CONFIG_TIMEOUT_VALUE_MS, 0x0000},
{PHHAL_HW_CONFIG_MODINDEX, PHHAL_HW_RC663_MODINDEX_I14443B},
{PHHAL_HW_CONFIG_ASK100, PH_OFF}
};
解決済! 解決策の投稿を見る。
你用的是最新版的NFC reader library吗?type B默认都是从106K开始通信的,如果你的应用是基于最新的NFC reader library的话,在通信过程中会根据PICC的应答设置成该卡支持的最大数据传输率,无需做上述的改动。
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
你用的是最新版的NFC reader library吗?type B默认都是从106K开始通信的,如果你的应用是基于最新的NFC reader library的话,在通信过程中会根据PICC的应答设置成该卡支持的最大数据传输率,无需做上述的改动。
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
谢谢!!