DISCLAIMER APPLICABLE TO THIS DOCUMENT CONTENTS:
This post contains a guide of how to use LPC55S69 demoboard with other NXP demoboards to demonstrate Access control using NFC, one embedded secure element and an MCU (see picture below). A ready to use package including preparation of a secure element, and of a MIFARE DESFire EV2 card can be used as 3-step authentication example using symmetric AES keys; a session key will be generated inside SE050 which will be exported to LPC55S69 which will handle contactless communication thru CLRC663 plus frontend.
This document is structured as follows:
Following hardware is required to run the project:
The LPCXpresso55S69 development board provides the ideal platform for evaluation of and development with the LPC55S6x MCU based on the Arm® Cortex®-M33 architecture. The board includes a high performance onboard debug probe, audio subsystem and accelerometer, with several options for adding off-the-shelf add-on boards for networking, sensors, displays and other interfaces.
The LPCXpresso55S69 is fully supported by the MCUXpresso suite of tools, which provides device drivers, middleware and examples to allow rapid development, plus configuration tools and an optional free IDE. MCUXpresso software is compatible with tools from popular tool vendors such as Arm and IAR, and the LPCXpresso55S69 may also be used with the popular debug probes available from SEGGER and P&E Micro.
The OM-SE050ARD is the flexible and easy-to-use development kit for the EdgeLock SE050 Plug & Trust product family. It can be used in various ways for example via the Arduino interface compatible to any board featuring an Arduino compatible header, including many i.MX, LPC and Kinetis boards, or via a direct I2C connection. This kit allows evaluation of the SE050 product family features and simplifies the development of secure IoT applications. More information can be found in the respective Application Note AN12395.
OM-SE050ARD | LPC55S69 (Conn.# - Pin #) | Port | Function Name |
SE_SDA (J22-1) | P24-6 also P17-3 | PIO1_21 | FC4_I2C_SDA_ARD |
SE_SCL (J22-4) | P24-5 also P17-1 | PIO1_20 | FC4_I2C_SCL_ARD |
+5V_PC (J22-2) | VDD_TARGET | ||
GND (J22-3) | GND |
Connect SE050 to LPC55S Arduino stackable headers and change jumper J14 as:
This connects SE_VDD directly to 3V3 and bypasses enable signal. This is required because enable pin on LPC55S coincides with Silex-2401 SPI pins so we cannot use SE_EN signal to drive SE_VDD.
It is easier to use the BLE-NFC-V2 board since less changes have to made on the board as compared to the CLEV6630B board.
The following figure shows the pin mapping between the two boards. It is advisable to add a pull-up resistor (4k7 to VCC) on CLRC663 plus signal IRQ.
The CLEV6630B board consists of CLRC663 plus (NFC frontend) connected by default to an LPC1769 µC via SPI. However, the board is made in such a way that the LPC1769 MCU can be bypassed to connect to an external MCU (in our case the LPC55S69) easily. For doing so:
The CLEV6630B is shown in Figure 2 after the required changes have been made to it (Removal of resistors and soldering of wires).
Now connect the two boards as follows:
Signal function | LPC55S69 (conn. # - Pin #) | Port | CLEV6630B |
MOSI | P17-10 | PIO0_20 | MOSI |
MISO | P17-12 | PIO0_19 | MISO |
SPI SCK | P17-14 | PIO0_21 | SCK |
SPI CSEL | P17-6 | PIO1_11 | SSEL |
RESET | P18-11 | PIO0_15 | CLRCL_NRST |
IRQ | P18-3 | PIO1_10 | IRQ |
GND | P17-7 | GND |
As final touch to this demonstrator, one LCD display will be added in order to show "access control" check result when approaching a MIFARE DESFire EV2 card to the Reader antenna, without the use of a computer console.
Connection between LPC55S69 board and LCD Display:
TFT | LPC55S69 (Jumper # - Pin #) | Port |
SPI_CLK | D13 (P17-9) | PIO1_2 |
SPI_MISO | D12 (P17-11) | PIO1_3 |
SPI_MOSI | D11 (P17-13) | PIO0_26 |
SPI_CS_TFT | D10 (P17-15) | PIO1_1 |
GPIO_LCD_BL | D9 (P17-17) | PIO1_5 |
GPIO_LCD_DC | D7 (P18-1) | PIO1_9 |
5V | 5V |
|
GND | GND |
|
Click here to order 2.8 inch TFT Display from Waveshare: P/N: 2.8 inch TFT Touch Shield Brand