Make the NFC reader library easier to read, by removing folders for the frontend ICs not needed in a project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Make the NFC reader library easier to read, by removing folders for the frontend ICs not needed in a project

Make the NFC reader library easier to read, by removing folders for the frontend ICs not needed in a project

The NFC reader library is supporting multiple frontends. For a customer this might become a more difficult to use, if only the part for one of the frontend chips is needed.

To enhance the readability and usability, you can remove the support for not used reader ICs by simply removing the folders below NxpRdLib/comps/phhalHw/src. For instance: if you only want to use the RC663, you could simply delete the folders Pn5180, Rc523. The result would be a library that only supports RC663.

This short screen recording shows the steps to reduce the number of supported Frontends.

标记 (1)
无评分
版本历史
最后更新:
‎04-14-2016 05:44 AM
更新人: