Hi there,
I have been back to high power design.
My system contains 3phase, 380V, 50Hz ac input, secondary surge protector, Aux Tr ( single phase, 380V/220V, 300VA), phase transformer( 3ph, 380v/12v,0v,12v,100VA) and a main transformer ( 3ph, 380V/9V,18V,800VA),
SCR(1600V, 50A) bridge, DC reactor( DC 20V,20A). Rectifier output should be DC 20V 20A.
My requested EVM should be,
1. PTR secondary windings phase, amplitude and rating controller.
2. MTRs secondary fuse (690V, 32 A) sensing
3. SCRs switching controller.
4. 50mlV, 30A shunt sensing,
5. GPS communication,
6. RSM
7. LAN
8. Display....etc,
Kindly recommend me one.
You can also transfer this post to suitable forum.
Regards
Have you looked at this Evaluation platform HVP-MC3PH. Here is a link to it.
It does not meet your exact requirements but it is the closest available solution.
Below I have copied an overview
The NXP® High-Voltage Development Platform is an evaluation and development solution for Kinetis® V Series MCUs and NXP Digital Signal Controllers.
Main board (power stage)
Regards,
Philip
Yes the schematic, the design files are available. Please go to nxp.com and search for HVP or use this link. Once there go to the Software and Tools tab and find the download link for the platform and each of the MCU evaluation boards.
Hello,
the HVP-MC3PH board provides analog sensing of:
Detail specification can be found in a board User's manual
Using these analog signals you should be able to implement features listed in your previous request to your application code.
Regards,
Pavel