S32K MBD-Toolbox generate code for IAR bug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K MBD-Toolbox generate code for IAR bug

1,053 Views
cg0
Contributor II

Hello,I use matlab 2018b, And I generate code for IAR, I already install the patch.

After generate code, I import the code to IAR for more coding, also I select the "S32K14x.icf" as Linker file. But it always run into fault. Because before I choose the .icf file from matlab, and this situation can run normally.

So, I replace the .icf file, it do works. Then I compare the two .icf file. The matlab generated .icf alway use S32K148 256k flash.icf, no matter what MCU selected.

Labels (2)
Tags (4)
0 Kudos
3 Replies

859 Views
constantinrazva
NXP Employee
NXP Employee

Hello cg0‌,

Thank you for your investigation! We will make this fix and provide a patch in the S32K Hotfixes page, but we'll do so most probably in May, after the Holidays are over.

Kind regards,

Razvan.

0 Kudos

859 Views
cg0
Contributor II

Hi Razvan

As I know  from https://community.nxp.com/thread/484197, the next version will be released this Q2. Could you tell me will S32K116/118 be added in?

0 Kudos

859 Views
constantinrazva
NXP Employee
NXP Employee

Hello cg0‌,

Indeed, S32K116/118 will be added in our next release.

Kind regards,

Razvan.

0 Kudos