MBDT License Activation was Failed in Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT License Activation was Failed in Linux

1,146件の閲覧回数
Mashiyojin
Contributor II

Hi Sir

Our team is using Linux OS Ubuntu 20.04 developing I.MX6 product for a while.

Now we are moving toward MBDT development of MPC5744p.

 

We have been trying to active the NXP's MBDT toolbox but failed.

Even we performs as ROOT user. the system does not see the license.dat file.

 

Can anyone suggest what should be a solution ?

 

BTW we use Ethernet IP address as HOST ID. since linux does not have DISK_SERIAL_NUMBER.

 

Thank you in advanced

Mashi Yojin

タグ(1)
0 件の賞賛
3 返答(返信)

1,099件の閲覧回数
Mashiyojin
Contributor II

I do not quite sure how the linux host pc(unbuntu) may  relate to the Andriod settings.

could you help explain more how to solve problem?

 

 

 

0 件の賞賛

1,133件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @Mashiyojin ,

Unfortunately, our toolbox is targeted only for Windows OS. I expect some functionalities to not work on Linux. 

However, your errors suggest that the in the lic folder (the one mentioned in the error message) is no .lic/.dat license file. You have to copy-paste the license file to that location.

You can give it a try on Linux to run or toolbox using a Windows emulator but we cannot provide support for that.

I am sorry for the inconvenience,

Marius

0 件の賞賛

1,099件の閲覧回数
Mashiyojin
Contributor II

The license file is already placed inside the folder follow the activation process.

however, the matlab plugin of nxp cannot find it even running program in Sudo.

0 件の賞賛